Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

   

I need to use some OPs and I'm not sure what kind of input I need now. Regarding to the colors of the OP-pin, I need an analog pin. But is this a hardwareconnection or not? Otherwise I thought about using a digital input pin with hardwareconnection enabled. If it is a real hardwareconnection, there shouldn't be any difference.

   

Seems to be an easy question but I'm a little bit stuck here.

   

 

   

Best regards

0 Likes
3 Replies
cadi_1014291
Level 6
Level 6
25 likes received 10 likes received 10 likes given

Hi, im not an expert but i had always used analog pins with the Opamps.

   

Guessing you are using a 5LP, the AppNote AN58304 describes the pins that we must use for best performance, and give us a table 3, in page 7:

   

http://oi61.tinypic.com/b5n0v7.jpg

   

   

i hope somebody can elaborate a better answer

   

Carlos

   

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

The term "Hardware Connection" for a pin (usually a digital pin) means that the pin is driven by an internal signal as opposed to driving the pin by software using a Pin_Read() or a Pin_Write() API.

   

Open the datasheet for the pin component and browse through the explanations for the parameters.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

This might be useful -

   

 

   

http://www.cypress.com/documentation/application-notes/an72382-using-psoc-3-and-psoc-5lp-gpio-pins      AN72382 - Using PSoC® 3 and PSoC 5LP GPIO Pins

   

 

   

Regards, Dana.

0 Likes