Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1

Anonymous
Not applicable

There is a KB article that mentions that a bug is there in the USB component in Psoc Designer. The same bug was found in USBFS in creator as well. KB article: http://www.cypress.com/?id=4&rID=38107  I have added some more analysis on the problem from the PC side.

The problem is that when a few packets of size 64 bytes is sent; the data is received, but not shown by the Hyperterminal/ any Serial Port Application. But when we constantly send a lot of data over the Hyperterminal in 64 bytes size packets, we are able to see that data on the Hyperterminal. This happens because the application has a buffer where it keeps the data and waits for a smaller size packet/ zero length packet to indicate the finish of transfer. If the data transferred is more than the buffer size, the data is displayed. This is what happens when you send a lot of data continuously on the USBUART.

This buffer size was found to be 4K for Tera Term and Cool Term Applications.
If you send suppose 3K bytes of data (in 64 bytes packets), you will not see the data displayed. Now, if you send another 3K bytes of data (in 64 bytes packets) you will see the first 4K data on the display of the application and the rest 2K would be in the buffer. To confirm this, now send 2K bytes of data (in 64 bytes packets). You will see 4K bytes of data getting displayed, with the last 2K as what you last sent.

Cheers.!!!

0 Likes
2 Replies
Bob_Marlowe
Level 10
50 questions asked 10 questions asked 1000 solutions authored
Level 10

A question:

   

Is Cypress taking over this DEVELOPER community? 35 post from you within 3 days giving us (the developers) answeres to questions we did not ask yet is more than a "normal" developer might swallow.

   

 

   

I thought (so far) that this community is for exchanging information and asking questions. I do not question at all the value of your information you present here, but it will get lost in the sea of postst here within a few months.

   

Quite a better place could be a well-tagges knowledge base integrated into this forum to pick the right information for the user who is in need of.

   

Correct me, if I am wrong: A community forum lives from dicussions, from the people and from the experiences the users made out-in-the-field, but your posts are mainly not an invitation for dicussing a subject but a pure information statement, valuable, a should-know, only misplaced.

   

 

   

Bob

0 Likes
MiRe_1607246
Level 2
Level 2

Hello, I have one question.

   

 

   

I made project with PSoC 5LP device (CY8C5868) and I need send data from chip using USBUART to matlab in debuging mode (I'm using miniprog3 for debuging ).

   

Problem is then windows 10 system is can't see device in debuging mode (I thing that windows will be disconnect my device from virtual com port when I'm using debuging). When I sent program to flash the comunication is work properly well. 

   

 

   

Do you know what can I do for using data transfer In debuging mode? 

   

 

   

 

   

Tnak you. Michal

0 Likes