Announcements

Ever wondered how you could shape the future in collaboration with others? Join us at OktoberTech Asia Pacific and get inspired. Click here to sign up FREE of charge.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

ZvVe_2582751
Level 1
First like given
Level 1

Hello,

In the sample USBFS_UART01 sample, one of the automatically generated sources is:

USBUART_episr.c

I want that my callback will be called upon an interrupt.

Should I modify USBUART_episr.c ?

I also added:

USBUART_EnableSofInt (); to main.c right after:

USBUART_Start

In general, how can I connect a specified interrupt in a device to my code ?

Thank you,

Zvika

0 Likes
1 Solution
AnkitaS_51
Employee
100 likes received 50 likes received 25 likes received
Employee

Hi,

Even when there is no active data transmission, the host uses Start of Frame (SOF) tokens to keep devices out of a suspend state.

In the ISR of particular EP you can use API "USBFS_GetEPCount()" which returns the current byte count from the specified USBFS endpoint.

It is dependent on your firmware that you write in callback.

View solution in original post

0 Likes
5 Replies
ZvVe_2582751
Level 1
First like given
Level 1

Hello,

Following is a fragment of the generated source.

Should I call my code (e.g giving a semaphore)  between the bold lines ?

Thank you,

Zvika

.....

#if (USBUART_SOF_ISR_ACTIVE)

    /*******************************************************************************

    * Function Name: USBUART_SOF_ISR

    ****************************************************************************//**

    *

    *  Start of Frame Interrupt Service Routine.

    *

    *

    *******************************************************************************/

    CY_ISR(USBUART_SOF_ISR)

    {

    #ifdef USBUART_SOF_ISR_ENTRY_CALLBACK

        USBUART_SOF_ISR_EntryCallback();

    #endif /* (USBUART_SOF_ISR_ENTRY_CALLBACK) */

       /* `#START SOF_USER_CODE` Place your code here */

        /* `#END` */

        USBUART_ClearSieInterruptSource(USBUART_INTR_SIE_SOF_INTR);

    #ifdef USBUART_SOF_ISR_EXIT_CALLBACK

        USBUART_SOF_ISR_ExitCallback();

    #endif /* (USBUART_SOF_ISR_EXIT_CALLBACK) */

    }

#endif /* (USBUART_SOF_ISR_ACTIVE) */

0 Likes
HeLi_263931
Level 8
100 likes received 50 likes received 25 likes received
Level 8

You can do that, but then your changes are lost on a clean build.

Better is to use

USBUART_StartEx(&YourISR);

in your main function (with your ISR routine defined with CY_ISR).

0 Likes
ZvVe_2582751
Level 1
First like given
Level 1

Hello,

Thank you for your reply.

In USBUART.h there is no declaration for USBUART_StartEx (...)

I tried to call this routine but got a link error.

I'm using Creator 4.0

Best regards,

Zvika

0 Likes
ZvVe_2582751
Level 1
First like given
Level 1

Hello,

Thank yo very much for your reply !

I'v noticed that the SOF ISR is called a lot (>1000) even if not a single character is sent from PC to the PSOC.

Can you tell why ?

I want to trigger a task (e.g with Semaphore) upon one or more characters sent to PSOC.

Thank you,

Zvika

0 Likes
AnkitaS_51
Employee
100 likes received 50 likes received 25 likes received
Employee

Hi,

Even when there is no active data transmission, the host uses Start of Frame (SOF) tokens to keep devices out of a suspend state.

In the ISR of particular EP you can use API "USBFS_GetEPCount()" which returns the current byte count from the specified USBFS endpoint.

It is dependent on your firmware that you write in callback.

0 Likes