Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

AlIa_1072791
Level 1
Level 1

Hi,

I've run the USBUART example with all the defaults for the CY8CKIT-030A kit and am having it send 256KB as fast as possible by looping transfer of 64 byte packets x 4096 times.

The issue is that USBUART seems to be pretty slow, it's doing about 160KB/s which is about 1.3Mbit transfer. Is this normal? I was hoping to achieve maybe 3Mbit or more.

Thanks!

Edit: I changed from Debug to Release compiling and that has sped it up a little bit more, 256KB/s. Is there anything else to make it faster?

0 Likes
1 Solution
Ekta
Moderator
Moderator
Moderator
250 solutions authored 100 likes received 250 sign-ins

Hi,

The USBUART component is implementation of a communications device class (CDC) USB interface. This is a USBFS Component with the descriptors configured to implement a CDC interface.

The CY8BKIT-033A supports Full speed USB. Thus according to the USB specifications the maximum effective data rate is 1.2 MBps.

The USBUART does not have any transfer rate limitation, but theoretically the transfer rate is limited by the USB Full Speed (12 Mbit/s- this is bus rate).

The effective data rate transfer is 1.2 Mbps (The actual data rates are affected by bus loading, transfer type, overhead, OS, and so forth).

For more details on this please refer to the page 11 of the USB 101 Appnote : https://www.cypress.com/file/134171/download

You can also refer to the USBUART section of the USBFS datasheet: https://www.cypress.com/file/376416/download

The above appnote also mentions the following:

pastedImage_0.png

Regards

Ekta

View solution in original post

1 Reply
Ekta
Moderator
Moderator
Moderator
250 solutions authored 100 likes received 250 sign-ins

Hi,

The USBUART component is implementation of a communications device class (CDC) USB interface. This is a USBFS Component with the descriptors configured to implement a CDC interface.

The CY8BKIT-033A supports Full speed USB. Thus according to the USB specifications the maximum effective data rate is 1.2 MBps.

The USBUART does not have any transfer rate limitation, but theoretically the transfer rate is limited by the USB Full Speed (12 Mbit/s- this is bus rate).

The effective data rate transfer is 1.2 Mbps (The actual data rates are affected by bus loading, transfer type, overhead, OS, and so forth).

For more details on this please refer to the page 11 of the USB 101 Appnote : https://www.cypress.com/file/134171/download

You can also refer to the USBUART section of the USBFS datasheet: https://www.cypress.com/file/376416/download

The above appnote also mentions the following:

pastedImage_0.png

Regards

Ekta