Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

Step 9 of the "Quick Start" section of "Bootloader Datasheet BootLdrUSBFSe V 1.30" reads, "After creating a project that compiles without errors, go to the Sample Firmware Code section. Modify and adapt the code given in the sample." I've looked for it, but can't find such a section, either in docs or the Workspace Explorer or the file system. Has the name changed, or am I just not looking in the right place?

   

There are a number of files with the name "bootldrusbfse_1_*.*" in the backup, lib, and lib\obj folders of my project. Is this what step 9 is referring to?

   

Thanks,
Doug Bell (VMC, contractor to Meteorcomm)

0 Likes
1 Reply
MYKZ
Employee
5 sign-ins First question asked 5 replies posted
Employee

If you've opened datasheet in PDF format, there is a section "Sample Firmware Source Code" on page 40, you'll see it in table of contents. It starts with "Create a new project with a base part supported by the BootLdrUSBFSe...".

   

Examples for HID Device and USB-UART (CDC) are given in this section.

   

   Misha

0 Likes