- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am using the psoc5.4 designer and created a project using an uart.
This project was working fine. Until I changed the paging attribute in the project settings.
My own code is only C I didn;t modify the assembler parts.
So I may expect that the uart_1.asm and uart_1int.asm are correct and do support the LMM.
When Paging is enabled I see the UART_1_bRxCnt getting a value.
But the UART_1_aRxBuffer is filled with 0x00
What should I do to get the LMM working in combination with the uart.
- Labels:
-
PSoC 1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Which PSoC device did you use?
LMM; I assumed it Cy8C29*** device.
Where is use that UART API?
In interrupt routine? or main polling loop?
or both combined?
Did you use context save and restore MACRO?
like this in the interrupt routine
... PRESERVE_CPU_CONTEXT
... lcall _ISRC_TxComplete
... RESTORE_CPU_CONTEXT
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Bob
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
I do not use the PRESERVER_CPU_CONTEXT
The uart is interupt enabled. Receiving is done by interupt.
And in my C code I check the UART_1_bRxCont
In include uartc.h function void uart_ontvangen(void)
I am however not able to debug with the ICE module. Because my psoc is togetter with other components in plastic.
So I can not connect to the psoc chip.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
That is first 256 byte, 0 - 255 byte.
If your buffer area is place without interrupt RAM area,
you can't access with it directly from interrupt routine.
So, you have to call these save/restore MACRO.
in_the_interrupt(void)
{
... PRESERVE_CPU_CONTEXT
... lcall _ISRC_UserProcess ;; CALL USER PROCESS
... RESTORE_CPU_CONTEXT
}
// USER CALL BACK ROUTINE //
void ISRC_UserProcess(void)
{
// access your buffer
... return;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Do I need to modify the uart_1.asm or uart_1INT.asm for that ???
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am not using an own (C code) Interup routine. So from the _UART_1_RX_ISR there is no call like you describe.
Maybe such a routine can be a workaround for my problem. (But then I need an example. how to implement such a routine.)
Because I am just a beginner in PSOC development.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
OK
This is a real code of my Cy8C29466 – UART
Something help for you.
;-------------------------------------------------------
; In the UARTINT.asm
;-------------------------------------------------------
_UART_RX_ISR:
;@PSoC_UserCode_BODY_2@ (Do not change this line.)
;
;---------------------------------------------------
; Insert a lcall to a C function below this banner
;---------------------------------------------------
PRESERVE_CPU_CONTEXT
lcall _ISRC_RxReady
RESTORE_CPU_CONTEXT
;---------------------------------------------------
; Insert a lcall to a C function above this banner
;---------------------------------------------------
;@PSoC_UserCode_END@ (Do not change this line.)
// ////////////////////////////////////////////////////
// this is a user process in main.c
// ////////////////////////////////////////////////////
volatile byte RxFlag, RxIdx, RxLen;
volatile byte RxBuf[UART_BUF_SIZE];
// ////////////////////////////////////////////////////
// in this routine, STX code 0x02 is start of record
// CR code 0x0D is end of record
// this routine handle only text data 0x20 ~
// ////////////////////////////////////////////////////
void ISRC_RxReady(void) // receive data ready
{ byte ss;
if( (UART_bReadRxStatus()&UART_RX_REG_FULL) && !(UART_bReadRxStatus()&UART_RX_ERROR) )
{ ss= UART_bReadRxData();
if( ss==STX )
{ RxIdx= 0; // if start text: clear pointer
}
else if( ss>=' ' ) // if text data
{ RxBuf[RxIdx++]= ss; // set buffer
if( RxIdx>=UART_BUF_SIZE-1 ) // if exceed data
{ RxIdx= UART_BUF_SIZE-1;
RxBuf[RxIdx]= 0; // complete buffer
RxLen= RxIdx;
RxIdx= 0;
RxFlag= 1; // record comleted
} }
else if( ss==CR ) // if end of text
{ if( RxIdx )
{ if( RxIdx>=UART_BUF_SIZE-1 ) RxIdx= UART_BUF_SIZE-1;
RxBuf[RxIdx]= 0; // complete buffer
RxLen= RxIdx;
RxIdx= 0;
RxFlag= 1; // record comleted
} } }
}
// ///////////////////////////////////////////////////////////////////
void UART_Initialize(void)
{ UART_Start(UART_PARITY_ODD); // Parity Odd
UART_EnableInt();
UART_IntCntl(UART_ENABLE_RX_INT); // Enable RX interrupts
}
// ///////////////////////////////////////////////////////////////////
byte UART_Receive( byte rec[], byte siz )
{ byte len;
if( !RxFlag ) return 0;
if( siz>=UART_BUF_SIZE-1 ) siz= UART_BUF_SIZE-1;
len= RxLen;
RxLen= 0;
if( siz<len ) len= siz;
strncpy( rec, (char*)RxBuf, len );
RxFlag= 0;
return len;
}
// ///////////////////////////////////////////////////////////////////
int main(void)
{ byte ss, rec[UART_BUF_SIZE];
UART_Initialize();
M8C_EnableGInt; // enable global interrupts
While(true)
{ if( ss=UART_Receive(rec, UART_BUF_SIZE) )
{
// do something using rec[]
} }
}
// ///////////////////////////////////////////////////////////////////
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content