cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

Hey all

   

I'm using the Psoc 5 and have instantiated the UART module v1.20. I noticed that after a call to USART_Start() i have to wait a bit before I can use PutChar or PutString. A delay of even just 1ms is enough, If no delay is present the first few characters are dropped. Any idea what's going on?

   

~Abhijit

   
0 Likes
1 Reply
Anonymous
Not applicable

Hi Abhijit,

   

 

   

It is recommended that you update to PSoC Creator v1.0 Production.

   

This version can be found at the following link http://www.cypress.com/?id=2494

   

 

   

The latest version of UART Component available is version 2.0.

   

So you can update the UART component to this latest version from v1.2 and give it a try.

   

PutChar() and PrintString() are Blocking Statements and hence doesn't require any delay to be used.

0 Likes