- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Forum,
i have made an 4 Channel-DMX Receiver with the PSoc5 Kit and it works fine with Interrupt based Code:
CY_ISR(ISR_DMX1)
{
// Check for break
if((UART_1_ReadRxStatus() & UART_1_RX_STS_BREAK) != 0)
{
DMX1Pointer = 0;
}
else //Read the Byte and store it in the Array
{
DMXIn1[DMX1Pointer] = UART_1_ReadRxData();
DMX1Pointer++;
}
}
Now i want to do this with DMA. I think there is no Problem to store the Bytes, but how do i reset the Stream when a Break of the UART is detected?
Günter
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You do not have any way to decide on DMA data transferred. You'll have to keep on using interrupts. Because of the comparable low speed of a UART there is no need using DMA, CPU stress is low.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hmm,
one DMX-Frame generates 514 Interrupts and is about 22,667ms long. So there are 1/0,022667 = 44,12 Frames per Second
44,12 * 514 = 22677 Interrupts per Second.
4 DMX Inputs and 1 Output = 113385 Interrupts per Second.
At least i try to make the DMX output with DMA.
Send the 513 Bytes, generate an Interrupt when all Bytes are copied and generate the Break in the Interrupt.
Then start DMA again.
Attached the Project. The Break is made with Delays in the Interrupt right now. The next Step is to replace this with a interruptbased PWM to avoid the Delays.
Günter
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
Hello Odissey,
the Delays in the Interrupt is fixed. I use a PWM Component to generate the Break and disconnect the TX with an AND during the BREAK.
I think the circular Buffer will also use Interrupts internally. So the amount will be the same, or is there a Hardwarebuffer?
Günter
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
Hello,
here are two Versions of the Code . The first one with Interrupts and the BREAK with an PWM-Component. This Code works, but i think it can optimized.
The second Code is my try to enable DMA for the TX Way, but it didnt work. I want to transmit 512 Bytes, one Byte after each OnTX-Complete. When all 512 Bytes are sent, an NRQ Interrupt of the DMA generates a BREAK. After this BREAK, DMA is started again. But now the DMA Dont start to transmit Data...
Günter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
3
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Three what?
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
#define DMADMX_SRC_BASE (CYDEV_SRAM_BASE)
#define DMADMX_DST_BASE (CYDEV_SRAM_BASE)
Source is not sram, but peripheral!
CyDmaTdSetConfiguration(DMADMX_TD[0], 512, DMADMX_TD[0], CY_DMA_TD_INC_SRC_ADR);
You should increment the destination, not the source.
CyDmaTdSetAddress(DMADMX_TD[0], LO16((uint32)&DMXOut[1]), LO16((uint32)UARTOUT_TXDATA_PTR));
You swapped source and destination.
I cannot see the place where you restart the DMA when finished.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Bob,
42!
The DMA is for TX. I want to send Data from Array to Uart.
#define DMADMX_SRC_BASE (CYDEV_SRAM_BASE)
#define DMADMX_DST_BASE (CYDEV_PERIPH_BASE)
How do i restart the DMA?
CyDmaChEnable(DMADMX_Chan, 1); //?
Günter
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
Hello,
is it possible to get seperate Interrupts from an UART Component? One for OnByteReceived and one for OnBreak?
Günter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
CyDmaChEnable(DMADMX_Chan, 1); //? Yes
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
now the Inputs also work with DMA. I used a Timer to detect the Break and fire an Interrupt, because i found no way to generate an seperate Interrupt onBreak in the UART Component.
Each Input has one Interrupt per Break (per Frame). The Output has two Interrups per Frame. One at the beginning of the Brake, on at the End of the Brake.
Günter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi every body.I have a question.why you use break generator in your project?can we use uart and dma alone to transfer data ?
because now i have a problem in my project . cpu has to work for several duty as CAN interface and adc and i2c and gsm and gps module.then transfer data on rs232 and gsm module.so if i dont use dma in my project,cpu is worked bad and data is being mixed up.
I think my big problem is transfer big data on rs232 quickly . how can i do cpu free from rs232?
please help me to solve this problem???
thanks for attention...