- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I'm a seasoned PSoC application designer. I'm using a PSoC 5LP. I have an application that uses the OpAmp v1.90.
Most of the time I need to configure the OpAmp with a mode = OpAmp. The '-' input is routed to an external pin of a current sense resistor. However due to the < 1Meg ohm input impedance (observed but not specified in the datasheet), I cannot resolve to < 30uA of current due to the extra draw and resultant noise.
If I "hard" configure the mode = Follower, I can resolve very low currents to ~ 1uA with much lower noise.
I want to configure the OpAmp to mode = OpAmp in the TopDesign and switch to mode=Follower in the code at run0time when needing to resolve to 1uA. I can operate at the register level if needed but it would be nice if there were some API calls to provide this.
Note: I tried using a analog mux external to the OpAmp to perform this desired function. I noticed many problems doing this successfully and had to abandon the attempt.
Thanks for the help in advance.
Len
"Engineering is an Art. The Art of Compromise."
Solved! Go to Solution.
- Labels:
-
PSoC 5 Architecture
-
PSoC 5LP
- Tags:
- opamp mode follower
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
In CYWDR you can see the switch address which enables the follower mode if you hover over the switch. Try writing this register run time.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Len,
can you explain how you measure 1uA current in Follower mode?
/odissey1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
odissey1,
The Opamp is being used as the power stimulus for the current sense circuit. When the stimulus is used in one mode (full scale range 0 to 20mA), I need +/- 100uA accuracy (Mode:OpAmp with an external pin connected to the '-' input). In another mode (Mode: Follower with NO external pin connection to '-' input), I need +/-1uA accuracy (full scale range 0 to 1.4mA). I can get this 1uA accuracy if I force this mode to Mode: Follower. I'm looking for a means to switch this Opamp mode setting on-the-fly at run-time to improve performance in the needed mode.
Len
"Engineering is an Art. The Art of Compromise."
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Len, I was hoping for a schematic, I can only guess about arrangement. Can you add a follower in front of "-" input of the opamp to serve as high-impedance input buffer?
Regarding the register access. I would file a case with Cypress support. But i wouldn't be much optimistic about their answer.
/odissey1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Here's two configurations I'm writing about. Each works to the accuracy I need if I 'hard' compile the schematic.
Len
"Engineering is an Art. The Art of Compromise."
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Len,
I would try to add a buffer in the feedback path, which should eliminate effect of low input impedance of the Opamp_1.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
user_342122993,
If I use the buffer (OpAmp_2) suggestion I run into the same issue since the input impedance of Opamp_1 '-' terminal is the same as the impedance of Opamp_2 '+' terminal (Note: The input impedance of these terminals are not specified by Cypress. They spec line exists but no value is stated). Additionally if I use another buffer between port P_2, it is prone to potential error due to gain and input offset errors. Therefore the output of Opamp_2 would be less accurate.
It comes to the idea that need a minimum of 4Meg input impedance in the mode when I want to measure 1uA resolution. Removing the internal connection to P_2 and configuring Opamp_1 to mode=Follower works because the P_2 has more than 4Meg isolation to the '-' terminal of Opamp_1 in this configuration.
Len
"Engineering is an Art. The Art of Compromise."
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
In CYWDR you can see the switch address which enables the follower mode if you hover over the switch. Try writing this register run time.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
user_411084576,
Thank you. I've done what you suggested. In addition, I needed to disconnect a switch previously connected to the '-' terminal as well otherwise the terminal is connected to two analog sources.
Len
"Engineering is an Art. The Art of Compromise."