- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
i looked forward to connect my PSOC 5LP with Tera Term, but Tera Term don't recognize any Port. PSOC Creator 4.2 recognize my PSOC 5LP and i can program it. I tried to press the Reset button like for 10 seconds but it didn't help.
Thanks
Best Regards
Tarik
Solved! Go to Solution.
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Tarik-san,
If you are using CY8CKIT-050, UART is not via KitProg.
So you (we) need either
(1) Use RS232 Interface on the board by connecting P12[6] and P12[7] to tx and rx socket. (May be opposite)
Then connect RS232 to USB adapter there and connect the adapter to your PC.
(2) Use USB-Serial adapter, connect Serial to P12[6] and P12[7] and connect USB to your PC
And either way, you (we) end up to connect "2" USB cables between the board and PC.
Another thing needed to be checked is, if you are using Windows 10, many USB-Serial adapters are not working
thanks for the "improvement" of MicroSoft, so please make sure that your USB-Serial adapter is compatible
with Windows 10.
Best Regards,
19-Oct-2019
Motoo Tanaka
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
(1) Which EVB are you using or you are using original board?
(2) If you are using CY8CKIT-050,
you need to connect P12[6] and P12[7] to tx and rx socket. (May be opposite)
If you are using CY8CKIT-059, have you assigned
UART_RX to P12_6
and
UART_TX to P12_7?
(3) Can you see the board or KitProg USB-UART in the Device Manager of Windows?
If not, please try
(3.1) Download and install the newest PSoC Programmer and install it.
https://www.cypress.com/documentation/software-and-drivers/psoc-programmer-archive
(3.2) Start PSoC Programmer and update firmware.
Please refer to the following topic.
Cannot fix firmware of CY8CKIT-044 progKit
(3.3) Quit PSoC Programmer and disconnect and re-connect the USB.
(4) Can you see the board or KitProg USB-UART in the Device Manager?
If so, note the COM number
and set TeraTerm Com from
Menu: Setup > Serial Port and chose Port: for the COM number
And also set the Speed to the speed you assigned in your PSoC Programmer UART Config.
If you are still in trouble, please let us know
- Which board you are using?
- How are you connecting the board to your PC?
Attached is my UART sample for CY8CKIT-059.
The baud rate is 115200.
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello moto,
thanks for answering.
(1) I using the original Board
(2) Using CY8CKIT-050,
I tired a lot to connect P12[6] and P12[7] to tx and rx socket. (May be opposite) but it didin't work.
(3) I see this in the device Manager from KitProg
(3.1),(3.2),(3.3) --> I have the newest version
I use CY8C5868AXI-LP035 100-TQFP
The Board is connected via USB to my PC-.
I think the Issue is as you see in the picture.
Best Regard
Tarik
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Tarik-san,
If you are using CY8CKIT-050, UART is not via KitProg.
So you (we) need either
(1) Use RS232 Interface on the board by connecting P12[6] and P12[7] to tx and rx socket. (May be opposite)
Then connect RS232 to USB adapter there and connect the adapter to your PC.
(2) Use USB-Serial adapter, connect Serial to P12[6] and P12[7] and connect USB to your PC
And either way, you (we) end up to connect "2" USB cables between the board and PC.
Another thing needed to be checked is, if you are using Windows 10, many USB-Serial adapters are not working
thanks for the "improvement" of MicroSoft, so please make sure that your USB-Serial adapter is compatible
with Windows 10.
Best Regards,
19-Oct-2019
Motoo Tanaka
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you. Tera Term recognized the serial port. But do you know how to send commands via UART. I use UART_PutString command, but i don't where to put the command.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
To begin with, could you take a look at my sample program?
tty_utils a utility sample for CLI type program
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Ok, i got it . It works.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
TaGe,
If you are using the 050-Eval board as it appears, you might find this useful.
In the link provide below, there is an link to source code that:
- Provides code to convert UART API calls for USBUART API calls and can use the 050 Eval board USB port. (This is what you are looking for).
- Provides a GetString() call to allow the user to only type in characters that match the String type required. Examples of types are Unsigned Decimal, Signed Decimal, Floating, Hexadecimal, FileSystem Name Strings and of course Strings.
- Provides example of of a single-character menu driven system that can be modified and expanded.
GetString() function that supports input character filtering. Includes menu-driven commands.
Len
"Engineering is an Art. The Art of Compromise."