- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am currently working on a board designed by a professor at my university using the microcontroller CY8C29466-24PXI, this board controls 12 motors (12 8bit PWMs), has 4 LEDs, 2 switches and 1 LCD display.
So far, using ¨PWMs I've made the robot walk on a straight line but without control, it begins walking as the board and the power source are both ON, so I need to use the two switches to start and stop the motion of the robot, and for that we thought to use one for each action, but I don't know how to integrate the button action to the Block diagram and the main.c code.
Also, I've assigned LED_1 and LED_2 to ports P1_2 and P1_3 respectively, but when i try to iniciate them from the main.c, they don't appear, I begin writting "LED_1_Start();" but the code helper does not show any LED connected.
Thanks beforehand to anyone that could help.
Solved! Go to Solution.
- Labels:
-
PSoC 1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Welcome in the forum!
It is always advisable to post your complete project, so that we all can have a look at all of your settings. To do so, use
Designer ->File-> Archive Project (minimal)
and attach the resulting .zip file.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Welcome in the forum!
It is always advisable to post your complete project, so that we all can have a look at all of your settings. To do so, use
Designer ->File-> Archive Project (minimal)
and attach the resulting .zip file.
Bob
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
I am using latest Designer 5.4 and the LED_1_Start() is shown in code completion (Did you switch it off?)
The program code looks a bit unstructured, better to use a self-written Delay() function instead of repeating the code-lines. Much better would be to use a timer, since the program could do different things until a timer fires its interrupt.
When you can write a function that performs a step of the robot, it would be easier to start and stop it with a button.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I now am able to program the start of LED1 and LED2 it may be because i didn't compile the code later, thanks.
About the delay, I am writting these methods:
void DelaySimple (void){
for (i=0;i<=30000;i++) {}
}
void DelayLong(void){
for (i=0;i<=30000;i++) {}
for (i=0;i<=30000;i++) {}
for (i=0;i<=30000;i++) {}
}
And using them like this:
PWM8_4_WritePulseWidth(11);
DelaySimple();
PWM8_5_WritePulseWidth(17);
DelaySimple();
PWM8_7_WritePulseWidth(17);
DelaySimple();
And is thowing me 5 errors and 38 warnings, can you please tell me why?, I've only coded before on JAVA and on void methods you don't put a return.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
your variable i is not declared within your functions.
and I would write
void DelayLong(void){
uint8 i;
for (i=0;i<;i++) {DelaySimple()}
}
Here is a link to my favourite C-manual
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Bob, when you say:
"When you can write a function that performs a step of the robot, it would be easier to start and stop it with a button."
How can i read the input from Port_1_0 and Port_1_1, when the button is pressed, my professor said that in a microcontroller an interruption the reading does not have to be in the code itself, but how then can I read that interruption? I was thinking if I can use the state on P1_0 like a boolean variable, so it can be used inside an if as the conditional,
i.e.:
while (1){
int decide;
if(Port1_0_Read()){
//Reads when SW1 is pressed
decide = 1;
}
if(decide==1){
//Robot code here
if(Port_1_1_Read()){
//Reads when SW2 is pressed
decide == 0;
LCD_1_PrCString("STOPPED");
}
}
}
But in code completion does not appear that Read() command, what command is simmilar to the one I need?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
When you read a mechanical switch like a push button you have
to debounce it. You can poll it or use an interrupt.
This ap note shows how to read a button. Also this shows how to use
shadow registers for read modify writes to the port.
http://www.cypress.com/?rID=2900 AN2094 - PSoC® 1 - Getting Started with GPIO
https://www.youtube.com/watch?v=tei6q5M3C0g Shadow Registers
http://www.cypress.com/?rID=39497 Shadow Registers
Link to ways of debouncing - www.dropbox.com/s/r8vfqea5fhiuzw1/Debounce.zip
Delay functions for PSOC 1 - www.cypress.com/
Regards, Dana.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
there are two things you have to solve: the electrical and the program.
A Button usually connects a pin to Vdd or to GND. to the pin must be connected to the opposite using a resistor. This can be done internal to the PSoC with the pin drive mode. Additionally you ought to give the pin a characteristical name as "StartButton".
Then the function StartButton_Read() will give you a value of the current input pin's voltage level, High or Low, TRUE or FALSE
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks Dana and Bob!
Bob, the board already came with the resistor needed for both switches, but I don't understand when you say:
"Then the function StartButton_Read() will give you a value of the current input pin's voltage level, High or Low, TRUE or FALSE"
I have the Port_1_2 and Port_1_3 assigned as the StartButton and StopButton respectively, but when I compile it, it does not show at the main in the code completion anything similar to StartButton_Read(). What am I doing wrong?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Read of a port is done like this -
uint8 myport1;
uint8 mypin3;
myport1 = PRT1DR; //PRT1DR is a macro in Designer for port1
Then you use a mask to extract the pin state. For example mask for pin 3
(pins numbered 0 - 7 in a port) = 0b00001000 = 0x08
So mypin3 = ( PRT1DR & 0X08 );
If you wanted mypin3 to be just a logical something like this -
mypin3 = ( PRT1DR & 0X08 ) ? 1 : 0;
The ap note posted earlier shows this.
Regards, Dana.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
...and to make things easier to read, thanks to the C preprocessor you may use
#define BitMask(BitNum) (0x01 << BitNum)
#define ReadPort(PortNo,BitNo) ((PRT ## PortNo ## DR & BitMask(BitNo))?1:0)
void main(void)
{
if(ReadPort(0,3)) HandleButtonPressed();
Bob