- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
I was planning to perform square wave voltammetry on a three-electrode configuration system. In square wave voltammetry, a symmetric square wave is superimposed with a staircase potential and then applied to a stationary electrode. I have decided to choose the PSoC 5LP board for this purpose. Therefore, can anybody provide any feedback or suggestions based on this? Is this board feasible to perform the experiment?
Thanking you
Solved! Go to Solution.
- Labels:
-
PSOC5 LP MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Aswin,
I have modified the project I provided earlier to more closely match the new requirements:
"The maximum current that needs to be sourced is mA at most. If it is a problem, then maybe 100uA.
as per requirement, each pulse is 50mV height, 25ms wide, applied in 5mV increment, with voltage resolution as -1 to +1V."
I added an ADC and compute an average Isense current for the circuit.
Attached is the modified project. I have not tested the project with the external resistors and connections. It does compile.
"Engineering is an Art. The Art of Compromise."