cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

The Cypress' charge controller based on CY8CLED04D01 has an in-built MPPT algorithmn. Is it possible to port that algorithm to a PSoC 1 device? Is there any advantage of using this device?

   

Sorry for posting the question again, I think I posted initially in the wrong location.

0 Likes
3 Replies
Bob_Marlowe
Expert II

No, you are right here, I answered one of your other threads here: http://www.cypress.com/?app=forum&id=1573&rID=73596 

   

 

   

Bob

0 Likes
ETRO_SSN583
Esteemed Contributor

http://www.cypress.com/?docID=34455

   

 

   

This ap note is accompanied by a project file set, written in C.

   

You could possibly port it to your own HW design.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

PowerPSoC has additional power peripherals like hysteretic controllers, CSA etc in addition to the core (which is same as the PSoC 1 core - M8C). Indeally, it should be possible to port the code to a PSoC 1 device but you will have to use external components. 

   

The key advantage of Cypress' solution is that it is is a single chip solution for battery charging and driving LEDs. PowerPSoC has 4 channels of the power peripherals, these can be used for LED driving as well. So, with one PowerPSoC device you can implement a single chip solution for charging the battery and driving LEDs.

   

You can find all the details about the Cypress's MPPT solution at the link - http://www.cypress.com/?rid=72393&source=header

   

The Application Note that Dana mentioned has all the details about this solution along with the firmware. The AN link is http://www.cypress.com/?rID=39126

   

Best Regards

   

Anshul

0 Likes