Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
BeS__284136
Level 3
Level 3
5 sign-ins 10 replies posted 5 replies posted

Hello.

   

The PSoC Creator is complaining that I cannot connect my analog GPIOs to both the DATA_SWITCHER multiplexer and the scanning comparator. See attached screen.

   

Error Message:

   

AMuxHW (Hardware Amux) only supports controlled analog connections to GPIOs. Please make sure all the controlled analog connections are connected to GPIOs.

   

I think the router is confused between the GPIOs and the inputs of the scanning comparator.

   

Is there any way to address this?

   

Thanks

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

The two scanning components use the same underlying switch matrix and so cannot be used in that configuration. A way out could be using two comparators, see attached picture.

   

 

   

Bob

View solution in original post

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

It would be much easier for us to test, when you provide us with a project archive.  To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.

   

 

   

Bob

0 Likes
lock attach
Attachments are accessible only for community members.
BeS__284136
Level 3
Level 3
5 sign-ins 10 replies posted 5 replies posted

Here is the project. Note it is a work in progress so the C code will not compile. Please do not mind that.

0 Likes
lock attach
Attachments are accessible only for community members.
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

The two scanning components use the same underlying switch matrix and so cannot be used in that configuration. A way out could be using two comparators, see attached picture.

   

 

   

Bob

0 Likes