I would like to copy SRAM data via DMA to the datapath FIFO. I am using the Datapath configurator. I want to use the FIFO F0.
So my plan was to use the f0_bus_stat signal to trigger the next DMA transfer if the FIFO is not full. The DMA is outside of this component.
I defined an output FIFObus_stat and mapped the signal f0_bus_stat to it -> ERROR invalid identifier
So what's the correct name of the f0_bus_stat signal?
Is there an example available that just shows what i want to do?
Solved! Go to Solution.
sorry, 2 min after posting i found the solution, you need to define this in the "Configure Datapath Outputs"
sorry, 2 min after posting i found the solution, you need to define this in the "Configure Datapath Outputs"