Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

HI there :

   

i use c8c29466. 

   

I have a SC Block works on data clock equal to20khz.

   

 Also ADC delsig8 works on data clock equal to 4Mhz, so it’s sample rate =4000000/256=15ksps.

   

I need to connect the output of SC Block to ADC but they have different clocks, and the output of an SC Block cannot be directly connected to the input of a CT block, cause the output of an SC Block is not continuous and is switching in nature.

   

How to connect the output of SCblock into input of ADC DELSIG internally and without use Analog bus  like use a adapter block or something i am unaware to ?

1 Reply
SampathS_11
Moderator
Moderator
Moderator
250 sign-ins 250 solutions authored 5 questions asked

Hello Ardamina,

   

The analog bus has to be connected in order to remove the switching frequency on the output of the SC block. This cannot be avoided.Kindly refer this KBA.

   

Sampath

0 Likes