- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I use a CY8CKIT-059 PSOC 5 LP Prototyping Kit.
The processor is running properly, when I use the internal clocks oran external XTAL on PIN 15.0 and 15.01.
Since internal clock and XTAL does not provide the required accuracy, I hav to use an external precise clock (e.g. 10 MHz TCXO).
Up to now we found no way to get the board running with an external clock.
I followed the following procedure:
1. Place a digital input pin in your top design.
2. draw a wire from that pin and give some name to that net.
3. In the .cydwr window, go to clocks tab and double-click 'master clock'.
4. A window named 'configure system clocks' will open. In this, check the 'Digital Signal' and click on the browse button.
5. Then select the net that you gave for the pin (clock input) previously and give the frequency and tolerance value.
6. Now you can use this clock to derive any clock source.
Do you have any idea, what could be the source of the problem?
Thanks in advance
Daniel
Solved! Go to Solution.
- Labels:
-
ispn:39618:1:0
-
l1:314:1:0
-
PSoC5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Welcome in the forum, Daniel.
I just checked out the configuration and it seemingly does work as expected. See attached project.
Did you scope your input clock?
Bob
PS: Where in Germany are you located? I live near Bremen.
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
Hello odissey, hello Bob,
thanks for yur quick answers.
Thanks to Bobs example I found the failure. I didn't activated the Input buffer for my clock Pin.
Now it works. Thanks a lot! 🙂
@Bob
I live in Ulm