cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

ShBa_282106
New Contributor II

Hi all!

   

This project is supposed to count all  pulses lying in an amplitude window in two parallel channels C1 and C2 for 10 seconds. Both C1 and C2 are supposed to report counts independently in their programmed window and keep updating  and displaying on PC through a USBUART interface.

   

One problem that has been persistent is that quite often one of the channels C1 or C2 measures 65535-n counts instead of n counts. It settles in some time but appears randomly. Default amplitude window for channel 1 is 1to 1.5V and for channel 2 is 2 to 2.5V. The data is attached as a text file as well as the project.

   

Please see

   

thanks

   

Neha

0 Likes
8 Replies
ShBa_282106
New Contributor II
0 Likes
Bob_Marlowe
Expert II

Two things come to my mind:

   

To start all counters at the same time you should use a control register, reset the counters and start them anew. Keep in mind that the reset-pulse is not asynchronous.

   

 

   

Check the count signals (route them to a pin) for ringing.

   

 

   

 

   

Bob

0 Likes
ETRO_SSN583
Esteemed Contributor

You need to sync all counter activity, not just the enable bit but also the VDAC

   

updates (eg. cntrs should be reset after VDAC update) so that they  are all

   

looking at the same window in time and V ? Or does that matter ? Also cntrs

   

should be all read when stopped (if window in time important).

   

 

   

Additionally you have configed as up cntrs, reloaded (65535) on Tc. Is that what you wanted ?

   

Seems that period value should be set to 0 in properties, not 65535 as you now have time set.

   

Seems like reload should not happen on Tc as well. And you don't need reload checked on

   

capture either.

   

 

   

Then in the DO loop you init() followed by a write() of 0. The init resets cntr to its properties values,

   

which is 65535, then you write 0x0000 to cntr. Seems like the init() did not accomplish much.

   

 

   

Lastly, if counts should exceed 16 bit value then you need to detect rollover in code or use a bigger

   

cntr.

   

 

   

Regards, Dana.

0 Likes
ShBa_282106
New Contributor II

Thnx Bob,

   

is it necessary to use a control register to reset the counters? Is there any other way throgh software?

0 Likes
ShBa_282106
New Contributor II

Thnx Dana,

   

Amplitude window should be fixed before the signal appears. Datasheet says it may take about 25us for DAC to settle and since counting time will be no less than 10 seconds, I dint put a delay. However if counters have to be reset after each update how do i do it in code? I dint see any Counter reset API 😞

   

And yes, all counters should look at the same window as i dint sample and hold the analog input. As soon as a delay of 10 seconds is over, all counters should be read and ready themselves for next counting if the signal lies in desired amplitude window.

   

Am not very clear how the period value setting will effect. Should it be set to zero? What should Reload counter settings be in this case? Pulses should be up counted from zero to a value it accumulates in 10 seconds such that counts per 10 seconds are reported.

   

Am not getting 65535-n problem if i subtract values from two counters only after checking that lesser is subtracted from greator. But that is not very appropriate to do as am not resetting the counter. Some times same values are repeated many times even if input pulses' amplitude is changed. Attaching the modified project

0 Likes
ShBa_282106
New Contributor II
0 Likes
Bob_Marlowe
Expert II

Re: ontrol register to start all counters:

   

It depends on how precise you want to start your counters synchronously. Some asm-instructions give a delay ín the range of a couple of µs, while a digital signal as coming from a control-register only gives a delay in the range of ns. It all depends on the speed of your clock, you may miss one pulse.

   

Resetting a counter is done in software as: Stop counter, write new counter value (zero for up-count 64K for down-count) then counter is considered to be resetted.

   

 

   

Bob

0 Likes
ETRO_SSN583
Esteemed Contributor

Your counters, set as up counter, period should be set to 0. You have them configed

   

to reload period when a reset = 0. So generate reset from a control register or a timer

   

fed to both counters.

   

 

   

You also have the reload set to Tc event. If you want capability to collect more than

   

65535 pulses, then either use wider counter, or test for rollover and add the additional

   

accounts when rollover detected. Note this would expand count to 2 X 65535. In this case

   

do not enable reload on Tc.

   

 

   

Additional sychronicity could be achived by using a sync module at the output of both

   

comparators, synced to bus clock. Of use a 10 sec timer to create a HW window to

   

trigger everything off. If you wanted to synch the VDACs Verilog solution only real

   

effective solution where simultaneous writes could occur to both VDACs from synced

   

registers.

   

VDAC settling time (large signal) is

   

 

   

0 Likes