Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

I am using two PSoC 5LP with two different sketches. The first PSoC simulate some SPI-Data-Transfer and the second should receive all Data.
The RX-Buffer should be cleared by the DMA. The SPIS-Rx-Int. is set on "Interrupt when FIFO not Empty".
The problem is that the Slave only receive the first Byte (Picture 1) and wont reset the Rx Interrupt (Picture 2).
My Sketch based on the SPIM/SPIS-DMA example from cypress.

SPI_RX_INT.jpg

CH8= DMA_Tx_Master

CH9= DMA_Rx_Slave

CH10=SPIS_Rx_Interrupt

SPI_RX_NO_INT.jpg

Did i forget some SPI config?

Is the timing for the SPIS-Interrupt correct at the 8th clock-rise?

Is there some kind of SPI-continously-receiving mode?

0 Likes
1 Solution
ShanmathiN_06
Employee
Employee
25 likes received 10 likes received First like received

Hi Eddi,

It looks like the descriptors are not chained properly.

In function Dma_S_Rx_Configuration(), modify the following,

CyDmaTdSetConfiguration(S_RxTD[0u], 1, S_RxTD[1u] , TD_TERMOUT0_EN|TD_INC_DST_ADR);

CyDmaTdSetConfiguration(S_RxTD[1u], 1, S_RxTD[0u], 0);

Also, SPIS_RX_STATUS_MASK_REG=1 (in ISR) and SPIS_EnableInt() (in main) are not necessary.

If "Interrupt on Rx FIFO not empty" is enabled in the SPI configuration window, it will automatically take care of the interrupt enable.

Thanks,
Shanmathi

View solution in original post

2 Replies
ShanmathiN_06
Employee
Employee
25 likes received 10 likes received First like received

Hi Eddi,

It looks like the descriptors are not chained properly.

In function Dma_S_Rx_Configuration(), modify the following,

CyDmaTdSetConfiguration(S_RxTD[0u], 1, S_RxTD[1u] , TD_TERMOUT0_EN|TD_INC_DST_ADR);

CyDmaTdSetConfiguration(S_RxTD[1u], 1, S_RxTD[0u], 0);

Also, SPIS_RX_STATUS_MASK_REG=1 (in ISR) and SPIS_EnableInt() (in main) are not necessary.

If "Interrupt on Rx FIFO not empty" is enabled in the SPI configuration window, it will automatically take care of the interrupt enable.

Thanks,
Shanmathi

Anonymous
Not applicable

Hey Shanmathi,

thank you for your comment.
This change solved the Interrupt Problem.

best regards

Eddi

0 Likes