Hi I'm connecting the following pressure sensor to my psoc using my psoc 5lp . I watched couple of tutorials on how to interface a pressure sensor and have looked at the ADC example on psoc website. My code is very similiar to the person on the youtube link below. I also have watched the following analog sensor for the arduino code but its not working. similiar psoc posts also couldn't help me solve the problem. The pressure is from alibaba, I have used the formula used by arduino community.
https://www.youtube.com/watch?v=IqHeLsDwxVY&ab_channel=AngelaSodemann
https://youtu.be/UrqPxwsPWGk - anlog pressure sensor in arduino
https://community.cypress.com/t5/PSoC-5-3-1-MCU/Bourns-analog-pressure-transducer/m-p/127862
Solved! Go to Solution.
This problem has been solved many times, so there shouldn't be any serious problems.
Check a few points:
1. Create / use a simple project with ADC DElSig with 10 bit resolution without using float.
- make sure that the measurement is working and is in the range> 0 <1000 bit.
2. The sensor signal should vary from 0.5V to 5V / 3.3V (check with a tester) аnd must be connected to the ADC input.
The archive of your project and the name / Datasheet of the sensor will help a lot
- it is always easier to continue what you started than to guess.
Evgeniy
Hi,
Could you please share the exact code you have used and adc settings. Could you elaborate your observations too ?
Best Regards,
Vasanth
I was wondering if you know any psoc5 tutor that could help me with my project?
Hi Vasanth,
The maximum pressure for my pressure sensor is 0.8Mpa. I wanted to read it in PSI or pressure bar becuase megapascal is too small. I therefore converted 0.8 Mpa to PSI which is 116. I'm using a 10 bit ADC , therefore the maximum readable number should technically be 921.4 and the lowest number 102.4 but when I blow on it nothing happens.
Did you run the ADC before polling? (see example codes for ADC DelSig)
ADC_DelSig_1_Start();
ADC_DelSig_1_StartConvert();
yes but that doesn't fix the problem. The LED keep flashing faster if I use the pressure as vaccum but that reading doesn't update in the LED.
This problem has been solved many times, so there shouldn't be any serious problems.
Check a few points:
1. Create / use a simple project with ADC DElSig with 10 bit resolution without using float.
- make sure that the measurement is working and is in the range> 0 <1000 bit.
2. The sensor signal should vary from 0.5V to 5V / 3.3V (check with a tester) аnd must be connected to the ADC input.
The archive of your project and the name / Datasheet of the sensor will help a lot
- it is always easier to continue what you started than to guess.
Evgeniy