Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

hara_4577791
Level 1
Level 1

Hello Team Members,

I am new to Cypress devices as well as community.

Currently i am searching on the PLCC solution over AC line @ 230V which we normally have at our home.

I want to transmit Audio signals over PLCC lines and receive same on the other end without any loss.

What can be the maximum data rate by which we can transfer audio signals?

Can you suggest such possible solutions which can support to transmit audio signals.

Which modulation technic will be supported for Audio signal transmission?

Let me know if you need more info.

Thanks

Hardik Raval

9924319427

0 Likes
1 Solution
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

Hardik,

Wire lines audio was popular some 20 years ago. Since then WiFi and Bluetooth took over as cheaper and safer alternatives.

For wire lines consider I2S or SPDIF for transmitting the data. There are some Cypress examples and some user examples on the forums.

/odissey1

View solution in original post

0 Likes
3 Replies
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

Hardik,

Wire lines audio was popular some 20 years ago. Since then WiFi and Bluetooth took over as cheaper and safer alternatives.

For wire lines consider I2S or SPDIF for transmitting the data. There are some Cypress examples and some user examples on the forums.

/odissey1

0 Likes

Hi Bota,

Can you please share me specific links than it would be more helpful for me to refer.

Getting more specific is that if i play Music on one end and that music after travelling over AC power-line i must be able to listen on the receiver end.

Is it possible to transmit such data in terms of music?

Please share your feedback.

Thanks & RegardsHardik Rawal

On Thursday, 14 November, 2019, 03:30:05 am IST, BoTa_264741 <community-manager@cypress.com> wrote:

#yiv7122200727 * #yiv7122200727 a #yiv7122200727 body {font-family:Helvetica, Arial, sans-serif;}#yiv7122200727 #yiv7122200727 h1, #yiv7122200727 h2, #yiv7122200727 h3, #yiv7122200727 h4, #yiv7122200727 h5, #yiv7122200727 h6, #yiv7122200727 p, #yiv7122200727 hr {}#yiv7122200727 .yiv7122200727button td {}

|

Cypress Developer Community

|

Powerline Carrier Communication for Audio Signals

reply from BoTa_264741 in Community Information - View the full discussion

Hardik.

Wire lines audio was popular some 20 years ago. Since then WiFi and Bluetooth took over as cheaper and safer alternative.

Consider I2S and SPDIF for transmitting the data. There are some examples here in the forums.

/odissey1

Reply to this message by replying to this email, or go to the message on Cypress Developer Community

Start a new discussion in Community Information by email or at Cypress Developer Community

Following Powerline Carrier Communication for Audio Signals in these streams: Inbox

This email was sent by Cypress Developer Community because you are a registered user.

You may unsubscribe instantly from Cypress Developer Community, or adjust email frequency in your email preferences

0 Likes

Hardik,

I don't have good links, please check this one

Re: Implement an UDP for getting a high frequency input

I believe that such project is advanced and not easy to implement. It will also require extra external hardware, such as codec to convert SPDIF into sound. I beliieve that WiFi is more promising.

/odissey1

0 Likes