Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

EmGa_3347101
Level 2
Level 2

Hi all!

I'm using a CY8CKIT-059 since few days with an USBUART block working without problems (show in PC terminal data from mcu).

But yesterday, I connected the USB cable and Windows 10 show me a driver error (device descriptor failure).

I programmed the same C8KIT with an USBUART example and it worked fine again...

But after, with my code again, doens't.

I'm using the default configuration of the USBUART block.

I don't  know why it broked.

I unistalled and re-installed PSoC Creator 4.2.

I select the driver from the folder of my project.

But doens't works.

1 Solution

The problem was in the main.

There was a funtion call writing in the usb uart before be correctly configured.

View solution in original post

0 Likes
6 Replies
Ekta
Moderator
Moderator
Moderator
First like given 250 solutions authored 100 likes received

Hello EmGa_3347101

You can try using the Microsoft Certified USBUART driver.

It can be obtained from the following link:

https://www.cypress.com/documentation/software-and-drivers/microsoft-certified-usb-uart-driver

Note: On Windows 10, you can use signed drivers only.

Please refer to the following thread regarding use of the driver: Re: Use of the Cypress Microsoft Certified USB UART Driver

Let me know if this works for you.

Regards

Ekta

0 Likes

Yes, I tried yesterday with this option too.

The same result. Driver error and no possiblity for installing it.

0 Likes
EmGa_3347101
Level 2
Level 2

.

0 Likes
Ekta
Moderator
Moderator
Moderator
First like given 250 solutions authored 100 likes received

Can you try using the following driver (see the path):

pastedImage_0.png

My project is working fine when using this driver.

Also can you attach the zip file for your complete project?

Regards

Ekta

0 Likes

Yes, I attached the project in my previous post.

Thanks for your support.

I select my project .inf file:

pastedImage_1.png

But, Windows doesn't use it!

pastedImage_0.png

0 Likes

The problem was in the main.

There was a funtion call writing in the usb uart before be correctly configured.

0 Likes