- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm developing a USB-CAN bridge using the PSoC5LP. I can see from http://www.cypress.com/?app=forum&id=2233&rID=87297 and also from http://www.cypress.com/?id=4&rID=58952 that the PSoC5LP does not require an external crystal for USB communications, unlike the PSoC5.
The TRM states that when using USB with the 5LP the IMO clock frequency spec is +/- 0.25%. This is up from the (best case) +/- 1% for IMO at 3MHz and +/- 4% at 24MHz when not using USB.
My question is whether the +/- 0.25% frequency accuracy is good enough for reliable CAN communications, or if I still require an external crystal to reliably communicate with CAN.
Solved! Go to Solution.
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
This might help in clock calulations -
http://cache.freescale.com/files/microcontrollers/doc/app_note/AN1798.pdf
Regards, Dana.