- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
We use DFB assembler component.
So we would like to use the firmware to load any constant in DFB RAMA into any CLC in DATA RAMA.
DFB_LoadDataRAMA(int32 * ptr, uint32 *addr, uint8 size);
It is speculated to use the above API.
We read the data sheet but do not understand it.
-- uint32 * ptr : pointer on the data source to load.
-- uint32 * addr : Start address for loading data into DFB RAM A. Is this a CLC (Current Location Couter)?
-- uint8 size : The number of data words to load.
Is the above recognition correct?
Please tell us what int32 * ptr, uint32 * addr, uint8 size mean.
Do you have sample code for this API?
Regards,
Solved! Go to Solution.
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi user_236195066,
Yes it is correct.
int32 * ptr is the pointer to the data (array) that you want to load into RAM A.
uint32* addr is the starting address to load data in the RAM
uint8 size: no of data words to load
You can refer to the code example attached that uses this API to load a value into the RAM A.
Hope this helps!
Regards,
Bragadeesh
Bragadeesh
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi user_236195066,
Yes it is correct.
int32 * ptr is the pointer to the data (array) that you want to load into RAM A.
uint32* addr is the starting address to load data in the RAM
uint8 size: no of data words to load
You can refer to the code example attached that uses this API to load a value into the RAM A.
Hope this helps!
Regards,
Bragadeesh
Bragadeesh
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Bragadeesh-san,
Thank you for confirming.
I also appreciate the sample code.
Regards,