Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
suleymaniye
Level 1
Level 1
First question asked Welcome!

I'm using CY8C29666 to generate two inverted PWM signals. That worked fine.

Now I want to enable and disable that PWM block using other PWM with much lower clock, like I show in the image.

suleymaniye_0-1623173148318.png

I connected the enable input of my PWMDB to the output of the other PWM,  but this is not working.

Previously, I've used a Counter to feed the Clock signal to an UART, so I expected this to work. Am I missing something on this? Any information would help.

Thanks

0 Likes
1 Reply
SampathS_11
Moderator
Moderator
Moderator
250 sign-ins 250 solutions authored 5 questions asked

Hello @suleymaniye ,

For troubleshooting this issue, can you kindly change the clock of PWMDB8_1 to VC2, and check if the PWMDB8 counts when enabled?

Best regards,

Sampath Selvaraj

0 Likes