Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
romac_285831
Level 2
Level 2

Can i turn off the IMO when the external clock is used to save power ?

0 Likes
2 Replies
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

The IMO is turned off in sleep -

   

 

   

http://www.cypress.com/?rID=34189

   

 

   

Regards, Dana.

0 Likes
MeenakshiR_71
Employee
Employee
100 likes received 50 likes received 25 likes received

Hello Rocky,

   

 

   

Though you can disable IMO, when using external clock by writing a '1' to the IMODIS bit in OSC_CR2 (refer TRM). It is not recommended, as disabling the IMO can cause flash read corruption over time and temperature. So the only recommended state to disable IMO is sleep state (which by the way automatically happens).

   

 

   

Regards,

   

MSUR