Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Anonymous
Not applicable

Hello Everybody,

   

I am using the ADC DelSig and I am afraid that the input voltage exceeds the voltage range programmed in psoc Creator. For Example, lets suppose that the voltage range is +- 1.024 V and my input voltage is 3V. If this happen, the psoc circuit is going to be damaged?

0 Likes
2 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

No damage as long as the input confirms to 0v <= Vin <= Vdd. the conversion result has to be examined thoroughly since it does not reflect a valid value and (afaik) might even be negative.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Ok, that's all I needed to know. Thanks Bob Marlowe!

0 Likes