Hi all,
Could someone please offer a good tutorial on how to port the FreeRTOS library onto the CY8C5888LTI-LP097 microcontroller? I was given one previously, however I was missing one file.
Solved! Go to Solution.
Hello,
Here are some references:
It explains how you can port FreeRTOS for PSoC4 devices. All the steps are similar for PSoC5 as well. Just note that you need to use the files in the ARM_CM3 folder instead of ARM_CM0.
Regards,
Dheeraj
Hello,
Here are some references:
It explains how you can port FreeRTOS for PSoC4 devices. All the steps are similar for PSoC5 as well. Just note that you need to use the files in the ARM_CM3 folder instead of ARM_CM0.
Regards,
Dheeraj
CaDu,
FreeRTOS has already been ported to the PSoC5LP. I've used this port many times.
There are a number of examples with FreeRTOS. There are also a number of discussions in the PSoC5LP forum as well as a few KBAs on this topic.
If you look to the right of this message box you should see a column named "More Like This"
In the column are links to other potentially related topics such as: PSOC 5LP FreeRTOS
Len
I created a very small, easier to use port of FreeRTOS to PSOC5, hosted on the CY8CKit-059 board.
It is available at https://github.com/wmaxfield/FreeRTOS-Minimal