Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi, I'm designing a 'hardware only' 3 channel DAQ system using an Analog Mux, DelSig ADC, and DMA. The ADC is hardware triggered at a 500us rate, with a channel sample rate about 20 times faster. (I'm sampling a 3PH power line). A uint16 by 3Channel by 1K circular software buffer is filled via DMA. The hardware and DMA are working just fine.

   

My problem is at some asynchronous time, a hardware interrupt is generated and I need to transfer the  ADC circular software buffer to another memory location for processing. To do this I need a Head Pointer into the buffer. The PSoC 4200M has the API function 'CyDmaGetDescriptorStatus' which returns the CYDMA_TRANSFER_INDEX from the Transaction Descriptor. I need this functionality from the PSoC 5LP DMA v1.70 component.

   

2nd, (less Important question) Is it possible to configure multiple linked TD's that would allow DMA to fill 3 separate uint16 by 1K circular ADC buffers, (one for each channel), so I don't have to deal with interleaved channel data in software? I have reviewed the 'DelSig_16Channel' example but it is 1-dimensional: (1 sample per channel), I need a 2-dimensional solution: ( 3ea 1K circular buffers).

   

Note: the ADC circular software buffer is always full, so I don't need a Tail Pointer, and I don't want any ISR involved with the hardware ADC sampling.

   

Any suggestions?

   

Thanks,

   

Gary Beam

0 Likes
1 Solution
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

2) Look at AN52705, example 5 - it explains how to chain TDs to fill two buffers in a page-mode.

   

1) you could read the TD data directly, it stores the current target address. AN84810 (advanced DMA topics) show how to modify a TD on-the-fly, you just need to do the reverse.

View solution in original post

0 Likes
1 Reply
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

2) Look at AN52705, example 5 - it explains how to chain TDs to fill two buffers in a page-mode.

   

1) you could read the TD data directly, it stores the current target address. AN84810 (advanced DMA topics) show how to modify a TD on-the-fly, you just need to do the reverse.

0 Likes