Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hello, 
I am working on a project with a CY8C5868-AXI-LP035 (also used in the 5LP module for CY8CKIT-001), 

   

This project has the real estate for only one port. So I am trying to use an USB micro connector (which has 5 pins). 

   

This allows me to connect a MiniProg 5pin conn appropriately  to the PSoC  for programming.

   

With proper routing, this leaves the USB data pins (2 & 3)  tied to  the PSoC SWD pins (15.6 & 15.7).

   

 

   

What I am trying to do now is use the USB data pins as a UART signal to a PC (ie a terminal or script program). 

   

However PSoC Creator 3.2 will not allow me to manually route pins 15.6 and 15.7 to the  UART Tx and Rx pins,

   

even when I choose System settings  Debug Select = GPIO,  Enable Device Protection = Yes. 

   

(Which is supposed to free the SWD pins for GPIO).

   

 

   

Can anyone suggest how I get Creator to use this pins for UART communication?

   

 

   

Additionally, on the CY8CKIT-001, are there any other contact points for the J9 USB connector other than the two white loop testpoints for Dp and Dm? I haven't found any ports that I can plug into...

   

 

   

 

   

Thanks for any advice.

   

ngohara

2 Replies
lock attach
Attachments are accessible only for community members.
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

This might help -

   

 

   

http://www.cypress.com/documentation/application-notes/an72382-using-psoc-3-and-psoc-5lp-gpio-pins      AN72382 - Using PSoC® 3 and PSoC 5LP GPIO Pins

   

 

   

Attached fixed pin constraints.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

Thank you for the advice.

0 Likes