Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

WaMa_286156
Level 5
Level 5
First comment on blog 100 replies posted 50 replies posted

After much trial and tribulation, I was able to get a design with several UDB counters and USBFS to route properly.  All Capture interrupts are occurring all the time, on a PSoC 5, along with using USBFS.

The key was to generate all of the timers and the rest of the design first.  After that, you can add the USBFS to the mix, and everything works.

If the USBFS was placed into the design first, then there were clock skew issues, and the input clock to the counters could only be about 12 MHZ.

  Also, if you want to debug faster and you are also using any fx2 based usb device, do the design in PSoC creator 3.3 or 4.0.  4.0 is much slower than 3.3, but 4.1 is glacial under certain circumstances.  However, the user interface to setting up the USBFS device is *much* better in PSoC creator 4.1.

0 Likes
2 Replies
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

can you please provide us with your project in order to recreate the issue at our end

0 Likes

I can, but it needs to be done privately.  Non disclosure if possible.

0 Likes