While programming the debugged code, message shows
"There was an error while programming the device: PSoC Programmer reported error (100 - PSoC Device (1E 02 80 69) is not in the DataBase)"
kindly suggest way out to update the data base
Solved! Go to Solution.
Hi Mr.Rakshith,
The problem is solved after reinstalling PSoC creator. Thanks for your initiative.
regards
V.Gopalakrishnan
Hi @Gopalakrishnan,
Can you please let me know the MPN of the PSoC 3 device that you are using? The device ID corresponds to CY8C3866AXI-040 and I see that the device ID is in the PSoC Programmer database.
Also, which version of PSoC Programmer are you using? Would it be possible for you to share a screenshot of the PSoC Programmer when the error occurs, on this thread?
Hi Mr.Rakshith,
The problem is solved after reinstalling PSoC creator. Thanks for your initiative.
regards
V.Gopalakrishnan