cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Gopalakrishnan
New Contributor

While programming the debugged code, message shows

"There was an error while programming the device: PSoC Programmer reported error (100 - PSoC Device (1E 02 80 69) is not in the DataBase)"

kindly suggest way out to update the data base

0 Likes
1 Solution
Gopalakrishnan
New Contributor

Hi Mr.Rakshith,

The problem is solved after reinstalling PSoC creator. Thanks for your initiative.

regards

V.Gopalakrishnan

View solution in original post

0 Likes
2 Replies
Rakshith
Moderator
Moderator

Hi @Gopalakrishnan

Can you please let me know the MPN of the PSoC 3 device that you are using? The device ID corresponds to CY8C3866AXI-040 and I see that the device ID is in the PSoC Programmer database.

Also, which version of  PSoC Programmer are you using? Would it be possible for you to share a screenshot of the PSoC Programmer when the error occurs, on this thread?

Thanks and Regards,
Rakshith M B
0 Likes
Gopalakrishnan
New Contributor

Hi Mr.Rakshith,

The problem is solved after reinstalling PSoC creator. Thanks for your initiative.

regards

V.Gopalakrishnan

0 Likes