PSOC5 LP

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

While I was checking on the data sheets of the creator 2.1 componets. 

   

I found the following table in the GraphicLCD spec

   

                                                                                                                                                                                                                                                

          

PSoC 3 (Keil_PK51)          

PSoC 5 (GCC)          

PSoC 5LP (GCC)          

Configuration         

Flash          

Bytes          

SRAM          

Bytes          

Flash          

Bytes          

SRAM          

Bytes          

Flash          

Bytes          

SRAM          

Bytes          

8-bit interface         

158         

1         

256         

5         

184         

1         

16-bit interface         

196         

1         

264         

5         

192         

1         

   

   

 

   

1. Looks like the 5LP is coming.

   

2. The flash size of PSOC5LP is different to PSOC5, Does that mean PSOC5LP has different instruction set or different hardware so the flash size is different?

0 Likes
1 Solution
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

AFAIK the LP version is a PSoC5 with higher peformance (e.g. the SAR ADC should have its 1Msps back). But it might be that it is the mysterious PSoC4, then it would have a M0 core. This would also explain the different code size. But who knows...

View solution in original post

0 Likes
3 Replies