- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello @MotooTanaka san,
I have been trying to get this example as a base to implement a simple HMI menu system using PSOC 5LP and 4x4 keypad and LCD: https://community.cypress.com/t5/Code-Examples/4x4-Matrix-Keypad-Sample/m-p/96977#M370
In the example code provided, the dump_key_matrix() function dumps the key pressed at that instant into a string str which can be used to print, either over UART or onto the LCD using appropriate functions (WORKS as described).
But, in a menu system, there are different levels at which the key press is to be detected (need to call dump_key_matrix() multiple times) which would mean that the dump_key_matrix() function needs to have a return type and not be 'void'.
I have tried modifying the return type to char and int too, where the letter[row][col] string will be used for a switch case and i set a variable flag with appropriate value for the corresponding key press, but this isn't working as intended.
Can you please guide me on how to modify the code to enable a return type for the dump_key_matrix() function which can be used to call the function multiple times in the code ( at different menu levels)?
To give a better view of what i want to implement:
1.) Show the first menu screen with 2 options to choose from (Press1 for Emp details, Press2 for Comp details).
2.) Take the input from user using dump_key_matrix().
3.) Based on the input, give the second menu screen with 2 more options to choose from.
If Press1 in first menu: Press1 for Name, Press2 for Age
If Press2 in first menu: Press1 for Company Address
4.) Again taking input from dump_key_matrix().
5.) Showing the third menu screen.
If Press1 in Second menu: emp_name (string)
If Press2 in Second menu: emp_age (string)
If Press 2 in first menu: show_company_details and address as a Up scrolling menu.
This is what i want to implement, but sadly i am not able to figure out the first part of getting a parsable (either using switch case or if else ) input variable to implement any of it.
Please help.
Regards,
Yash
Solved! Go to Solution.
- Labels:
-
PSOC5 LP MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Yash-san,
To accomplish a target, there can be infinite number of methods.
So the following is a sketch of mine and is not the only method to realize something you wish.
Having said that the following seems to be working (using UART)
#include "project.h"
#include "stdio.h"
#define NUM_ROW 4
#define NUM_COL 4
volatile uint8_t key[NUM_ROW][NUM_COL] = { 0u } ;
uint8_t letter[NUM_ROW][NUM_COL] = {
{ '1', '2', '3', 'A' },
{ '4', '5', '6', 'B' },
{ '7', '8', '9', 'C' },
{ '*', '0', '#', 'D' }
} ;
volatile int row_no = 0 ;
volatile int col_no = 0 ;
void scan_key_matrix(void)
{
switch(row_no) {
case 0: ROW0_Write(1) ; ROW1_Write(0) ; ROW2_Write(0) ; ROW3_Write(0) ; break ;
case 1: ROW0_Write(0) ; ROW1_Write(1) ; ROW2_Write(0) ; ROW3_Write(0) ; break ;
case 2: ROW0_Write(0) ; ROW1_Write(0) ; ROW2_Write(1) ; ROW3_Write(0) ; break ;
case 3: ROW0_Write(0) ; ROW1_Write(0) ; ROW2_Write(0) ; ROW3_Write(1) ; break ;
default: ROW0_Write(0) ; ROW1_Write(0) ; ROW2_Write(0) ; ROW3_Write(0) ; break ;
}
switch(col_no) {
case 0: key[row_no][col_no] = COL0_Read() ; break ;
case 1: key[row_no][col_no] = COL1_Read() ; break ;
case 2: key[row_no][col_no] = COL2_Read() ; break ;
case 3: key[row_no][col_no] = COL3_Read() ; break ;
}
col_no++ ;
if (col_no >= NUM_COL) {
col_no = 0 ;
row_no = (row_no + 1) % NUM_ROW ;
}
ROW0_Write(0) ;
ROW1_Write(0) ;
ROW2_Write(0) ;
ROW3_Write(0) ;
}
CY_ISR(my_tick_isr)
{
scan_key_matrix() ;
}
#define STR_LEN 64
char str[STR_LEN+1] ;
void print(char *str)
{
UART_PutString(str) ;
}
void printc(char c)
{
UART_PutChar(c) ;
}
void cls(void)
{
print("\033c") ; /* reset */
CyDelay(20) ;
print("\033[2J") ; /* clear screen */
CyDelay(20) ;
}
void splash(void)
{
cls() ;
print("5LP 4x4 Matrix Key Test") ;
snprintf(str, STR_LEN, "(%s %s)\n", __DATE__, __TIME__) ;
print(str) ;
}
void init_hardware(void)
{
CyGlobalIntEnable; /* Enable global interrupts. */
UART_Start() ;
splash() ;
CySysTickStart() ;
CySysTickSetCallback(0, my_tick_isr) ;
}
uint16_t get_key_matrix(void)
{
int col, row ;
uint16_t value = 0 ;
for (row = 0 ; row < NUM_ROW ; row++) {
for (col = 0 ; col < NUM_COL ; col++) {
value <<= 1 ;
if (key[row][col]) {
value |= 0x01 ;
}
}
}
return( value ) ;
}
void print_key_table(uint16_t key_table)
{
int row, col ;
uint16_t mask = 0x8000 ; /* bin: 1000_0000_0000_0000 */
snprintf(str, STR_LEN, "0x%04X: ", key_table) ;
print(str) ;
if (key_table & 0x8000) {
print("1 is pushed ") ;
}
if (key_table & 0x4000) {
print("2 is pushed ") ;
}
print("\n\r") ;
for (row = 0 ; row < NUM_ROW ; row++) {
for (col = 0 ; col < NUM_COL ; col++) {
if (key_table & mask) {
snprintf(str, STR_LEN, "%c ", letter[row][col]) ;
print(str) ;
} else {
print("_ ") ;
}
mask >>= 1 ;
}
print("\n\r") ;
}
}
#define BUTTON_1 0x8000
#define BUTTON_2 0x4000
#define BUTTON_D 0x0001
#define MENU_TOP 0u
#define MENU_10 10
#define MENU_11 11
#define MENU_12 12
#define MENU_20 20
#define MENU_21 21
#define MENU_22 22
int menu_mode = MENU_TOP ;
void greeting(void)
{
cls() ;
print("WELCOME TO THE") ; print("\n\r") ;
print("EMP/COMP DBS") ; print("\n\r") ;
}
void go_menu_top(void)
{
cls() ;
print("P1-Emp Details"); print("\n\r") ;
print("P2-Comp Details"); print("\n\r") ;
menu_mode = MENU_TOP ;
}
void go_menu_10(void)
{
cls() ;
print("PRESS 1: NAME"); print("\n\r") ;
print("PRESS 2: AGE"); print("\n\r") ;
menu_mode = MENU_10 ;
}
void go_menu_11(void)
{
cls() ;
print("Employee Name"); print("\n\r") ;
print("Yash"); print("\n\r") ;
menu_mode = MENU_11 ;
}
void go_menu_12(void)
{
cls() ;
print("Employee Age"); print("\n\r") ;
print("24"); print("\n\r") ;
menu_mode = MENU_12 ;
}
void go_menu_20(void)
{
cls() ;
print("Press1:Comp Name"); print("\n\r") ;
print("Press2:Comp Addr"); print("\n\r") ;
menu_mode = MENU_20 ;
}
void go_menu_21(void)
{
cls() ;
print("Company Name:"); print("\n\r") ;
print("ATPL"); print("\n\r") ;
menu_mode = MENU_21 ;
}
void go_menu_22(void)
{
cls() ;
print("Company Addr:"); print("\n\r") ;
print("Hyd"); print("\n\r") ;
menu_mode = MENU_22 ;
}
void do_menu_top(uint16_t key_table)
{
switch(key_table) {
case BUTTON_1: go_menu_10() ; break ;
case BUTTON_2: go_menu_20() ; break ;
default: go_menu_top() ; break ;
}
}
void do_menu_10(uint16_t key_table)
{
switch(key_table) {
case BUTTON_1: go_menu_11() ; break ;
case BUTTON_2: go_menu_12() ; break ;
case BUTTON_D: go_menu_top() ; break ;
default: go_menu_10() ; break ;
}
}
void do_menu_11(uint16_t key_table)
{
switch(key_table) {
case BUTTON_1: go_menu_11() ; break ;
case BUTTON_2: go_menu_11() ; break ;
case BUTTON_D: go_menu_10() ; break ;
default: go_menu_10() ; break ;
}
}
void do_menu_12(uint16_t key_table)
{
switch(key_table) {
case BUTTON_1: go_menu_12() ; break ;
case BUTTON_2: go_menu_12() ; break ;
case BUTTON_D: go_menu_10() ; break ;
default: go_menu_12() ; break ;
}
}
void do_menu_20(uint16_t key_table)
{
switch(key_table) {
case BUTTON_1: go_menu_21() ; ; break ;
case BUTTON_2: go_menu_22() ; break ;
case BUTTON_D: go_menu_top() ; break ;
default: go_menu_20() ; break ;
}
}
void do_menu_21(uint16_t key_table)
{
switch(key_table) {
case BUTTON_1: go_menu_21() ; break ;
case BUTTON_2: go_menu_21() ; break ;
case BUTTON_D: go_menu_20() ; break ;
default: go_menu_21() ; break ;
}
}
void do_menu_22(uint16_t key_table)
{
switch(key_table) {
case BUTTON_1: go_menu_22() ; break ;
case BUTTON_2: go_menu_22() ; break ;
case BUTTON_D: go_menu_20() ; break ;
default: go_menu_22() ; break ;
}
}
int main(void)
{
uint16_t key_table = 0 ;
uint16_t prev_key = 0 ;
init_hardware() ;
greeting() ;
CyDelay(3000) ;
go_menu_top() ;
for(;;)
{
key_table = get_key_matrix() ;
if ((key_table != 0) && (key_table != prev_key)) {
switch(menu_mode) {
case MENU_TOP: do_menu_top(key_table) ; break ;
case MENU_10: do_menu_10(key_table) ; break ;
case MENU_11: do_menu_11(key_table) ; break ;
case MENU_12: do_menu_12(key_table) ; break ;
case MENU_20: do_menu_20(key_table) ; break ;
case MENU_21: do_menu_21(key_table) ; break ;
case MENU_22: do_menu_22(key_table) ; break ;
default: menu_mode = MENU_TOP ; break ;
}
CyDelay(500) ;
}
prev_key = key_table ;
}
}
Best Regards,
1-Jul-2021
Motoo Tanaka