Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
keli_3765301
Level 1
Level 1

hi all:

    I have a design with CY8C5868AXI-LP035 to realize DAC ,ADC.

It can work below 60℃ and can't work when the ambient temperature rises to 75℃.

I use CY8C5888AXQ-LP096 to repalce  CY8C5868AXI-LP035 and the result is the same.

0 Likes
3 Replies
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

How do you judge that the chip doesn't work if the ambient temperature rises to 75 ℃?

What's the state of the chip, broken or recoverable?

Where did you buy these chips?

0 Likes

Thank you for the reply

1. The PCB works in High and low temperature test chamber. When temperature set to 25℃ ,it works well.

2. Chip is brand new.

3.Purchase through an agent

0 Likes
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

Keli,

What specifically doesn't work? 

As LinglingG said: Is the chip broken @ 75C? 

If the problem is that the DAC, ADC or other subsystems go out of spec, there may be solutions that could be exercised.

Len

Len
"Engineering is an Art. The Art of Compromise."
0 Likes