Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

CaDu_3933941
Level 4
Level 4
50 replies posted 25 replies posted 10 replies posted

Hi all,

I am considering using FreeRTOS for my project. I will need this program to be hard real time.

My problem is, I do not know where to start. How do I port the FreeRTOS API onto PSoC Creator?

1 Solution
user_3716231
Level 4
Level 4
10 sign-ins 5 sign-ins 10 questions asked

You need to download source code of freertos and add them into your project.

1.add freertos path into your project:

step1.png

2.create freertos folders:

step2.png

3.add existing freertos files into folders:

step3.png

4.add these code in your project

extern void xPortPendSVHandler(void);

extern void xPortSysTickHandler(void);

extern void vPortSVCHandler(void);

#define CORTEX_INTERRUPT_BASE          (16)

void FreeRTOS_Start(){

  

    /* Handler for Cortex Supervisor Call (SVC, formerly SWI) - address 11 */

    CyIntSetSysVector( CORTEX_INTERRUPT_BASE + SVCall_IRQn,

        (cyisraddress)vPortSVCHandler );

  

    /* Handler for Cortex PendSV Call - address 14 */

CyIntSetSysVector( CORTEX_INTERRUPT_BASE + PendSV_IRQn,

        (cyisraddress)xPortPendSVHandler );  

  

    /* Handler for Cortex SYSTICK - address 15 */

CyIntSetSysVector( CORTEX_INTERRUPT_BASE + SysTick_IRQn,

        (cyisraddress)xPortSysTickHandler );

}

View solution in original post

0 Likes
2 Replies
user_3716231
Level 4
Level 4
10 sign-ins 5 sign-ins 10 questions asked

You need to download source code of freertos and add them into your project.

1.add freertos path into your project:

step1.png

2.create freertos folders:

step2.png

3.add existing freertos files into folders:

step3.png

4.add these code in your project

extern void xPortPendSVHandler(void);

extern void xPortSysTickHandler(void);

extern void vPortSVCHandler(void);

#define CORTEX_INTERRUPT_BASE          (16)

void FreeRTOS_Start(){

  

    /* Handler for Cortex Supervisor Call (SVC, formerly SWI) - address 11 */

    CyIntSetSysVector( CORTEX_INTERRUPT_BASE + SVCall_IRQn,

        (cyisraddress)vPortSVCHandler );

  

    /* Handler for Cortex PendSV Call - address 14 */

CyIntSetSysVector( CORTEX_INTERRUPT_BASE + PendSV_IRQn,

        (cyisraddress)xPortPendSVHandler );  

  

    /* Handler for Cortex SYSTICK - address 15 */

CyIntSetSysVector( CORTEX_INTERRUPT_BASE + SysTick_IRQn,

        (cyisraddress)xPortSysTickHandler );

}

0 Likes
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on KBA 1000 replies posted 750 replies posted

Hi,

Last time, when I ported an older version of FreeRTOS to PSoC4, it was not very easy.

So Today, I googled "FreeRTOS PSoC 5LP" and found the following nice site.

(It is in Japanese, though)

https://tshell.hatenablog.com/entry/2019/05/23/212250

So I followed the instruction in that site.

(1) Download FreeRTOS from

FreeRTOS - Free RTOS Source Code Downloads, the official FreeRTOS zip file release download

I clicked the Green Button in the FreeRTOS box.

000-FreeRTOS-site.JPG

(2) Expanded the downloaded "FreeRTOSv10.4.1.zip"

    Folder "FreeRTOSv10.4.1" was created.

(3) In the Folder I digged int "FreeRTOS"

001-FreeRTOSv10_4_1.JPG

(4) I found "CORTEX_CY8C5888_PSoC_Creator_GCC" in FreeRTOSv10.4.1\FreeRTOS\Demo

002-FreeRTOS_Demo.JPG

(5) I double clicked the workspace

003-CORTEX_CY8C5888_PSoC_Creator_GCC.JPG

(6) Warning about the device used was obsoleted, proceeded by selecting "OK"

004-Obsolete_Device_Warning.JPG

(7) In the PSoC Creator, I selected "Device Selector..."

005-Device-Selector.JPG

(8) I selected CY8C5888LTI-LP097 for my CY8CKIT-059

006-select-097.JPG

(9) In the schematic, I see a lots of outdated components

007-schematic-01.JPG

(10) I selected "Update Components..."

008-Update_components.JPG

(11) Components were updated, and the schematic seems to be sane.

009-schematic-updated.JPG

(12) Pins

I only specifed

Rx_1: P12[6]

Tx_1: P12[7]

Pin_LED_0: P2[1]

Startup_Release_Switch: P2[2]

And left the rest as not "unlocked"

010-Pins.JPG

(13) Tera Term Log

After compiled and started the debugger, Serial port (57600) showed the following.

And according the the site referenced, this is the expected output.

011-TeraTerm-log.JPG

So the good news is porting or getting a version of FreeRTOS to 5LP was not as difficult as I was afraid of.

And the bad (or reasonable) news is that you need to learn the manner of using this RTOS to command it for your purpose.

moto

This widget could not be displayed.
This widget could not be displayed.