PGA output pin voltage not rising above 4V with change in input voltage

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Analog DAC output voltage swing is not raising above 4V. I used voltage DAC and PGA with gain of 4. I set 1V from DAC output to PGA input I am getting 4V. When I increase the PGA input to 1.2V I am still getting 4V. Do I need to add a pull down resistor is 10k at the  analog output pin driven by PGA

0 Likes
1 Reply
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

I believe that PGA needs at least 0.6V headroom to operate. It will not produce 4.8V.

0 Likes