- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am using a ILI9341 240x320 LCD Controller configured for Parallel indirect interface with a Touch screen. I do not know whether to add the nosts or osts directory to the compiler from the Include directory. Also, do not know which file to add to the linker, libemWin_nosts_cm3_gcc.a or libemWin_osts_cm3_gcc.a from the GCC directory. I guess this depends on whether I am using RTOS but not sure not sure how to determine whether I am or not. There is the question of which GUI_X Source file to use, GUI_X.c, GUI_X_FreeRTOS.c, GUI_X_embOS.c or GUI_X_uCOS.c from the FlexColor directory.
Any suggestion, Thanks Mike
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Please refer to the Segger Graphics Library User Guide to understand what files to include based on your application. The terminologies are as follows:
(1) nosnts --> No OS no Touch Screen
(2) nosts --> No OS but supports Touch Screen
(3) osts --> Support both OS and Touch Screen
The same applies to linker files, look at the naming schemes. For ex: libemWin_nosts_cm3_gcc.a.
Now coming to the next part of choosing the driver templates, please refer to the documentation available with the Segger Emwin Package. Once downloaded, it will be available at this path: "emWinGraphics_v5_46\Documentation\PSoC4_5"
In your case, your display controller ILI9341 is supported in GUIDRV_FlexColor as seen below:
So, in the FlexColor directory, the files to choose is again mentioned in the Segger User Guide Page#6:
Whether you want to use RTOS or not is completely your choice. If you aren't familiar with RTOS, then you need not use it.
Regards,
Dheeraj