Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hi,

   

I think I've got a problem with the new EEPROM 3.0 API. I used the old EEPROM API in other projects without problems:

   
For writing a Byte I used:     EEPROM_ByteWrite(someByte , 0x00,0x02);          for reading a Byte I used:        someByte  =  CY_GET_REG8(CYDEV_EE_BASE + 0x02);
   

That worked well and everything was good.

   

Now I tried to use the new API:

   
For writing a Byte I'm using:    EEPROM_WriteByte(someByte ,3);  for reading a Byte I'm using:        someByte = EEPROM_ReadByte(3);
   

Sometimes this works, sometimes not...

   

Do I use the new EERPOM API correct? Is that correct to not use the CYDEV_EE_BASE anymore? By the way, I'm using also I2C in my Project, I have no problem with that until I'm using the EEPROM.  Or are there any timing issues between I2C and EEPROM access?

   

thanks a  lot

1 Solution
Anonymous
Not applicable

Hi,

   

Can you refer to EEPROM code example provided with Creator ? You can find it here. Go to PSoC Creator -> File -> Code Example

   

What was the EEPROM component versions when it worked and when it did not ?

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Hi,

   

Can you refer to EEPROM code example provided with Creator ? You can find it here. Go to PSoC Creator -> File -> Code Example

   

What was the EEPROM component versions when it worked and when it did not ?

0 Likes