Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

PSoC3 CY8C34 Famiry

    DC Specifications

        VDDD (Digital core regulator enabled)  :  Min 1.8V  Max 5.5V

    Precise Low-Voltage Reset (PRES) with Brown Out DC Specifications

        PRESR (Rising trip voltage)  :  Min 1.64V   Max 1.68V

        PRESF (Falling trip voltage) :  Min 1.62V   Max 1.66V

PSoC4 PSoC4000S Famiry

    DC Specifications

        VDD (Internally regulated supply)  :  Min 1.8V  Max 5.5V

    Power On Reset (PRES)

        VRISEIPOR (Rising trip voltage)  :  Min 0.80  Max 1.5V

        VFALLIPOR (Falling trip voltage) :  Min 0.70V  Max 1.4V

Q1. when the voltage drops, PRES is asserted in PRESF(VRISEIPOR) voltage range.

    When the voltage recovers, PRES is negated in PRESR(VFALLIPOR) voltage range.

    Are these correct?

Q2. When the voltage drops, even if it is below 1.8V, the device is in the normal operating state until PRES is asserted.

    When the voltage recovers, even if it is still below 1.8V, the device is in the normal operating state after PRES is negated.

    Are these correct?

0 Likes
1 Solution
Anonymous
Not applicable

Yes, your interpretation is correct. When we say PRESF (Falling trip voltage) :  Min 1.62V   Max 1.66V - if VCCD or VCCA drops to anywhere between 1.62V and 1.66V, a PRES reset shall be asserted. Until PRES is asserted - the device shall be in normal operating range, but we do not guarantee full performance if voltage is between 1.66 V and 1.8 V.

View solution in original post

0 Likes
2 Replies
Anonymous
Not applicable

Yes, your interpretation is correct. When we say PRESF (Falling trip voltage) :  Min 1.62V   Max 1.66V - if VCCD or VCCA drops to anywhere between 1.62V and 1.66V, a PRES reset shall be asserted. Until PRES is asserted - the device shall be in normal operating range, but we do not guarantee full performance if voltage is between 1.66 V and 1.8 V.

0 Likes
Anonymous
Not applicable

Thank you for your answer.

Please tell me a little more.

What kind of performance degradation can it have?

0 Likes