Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

DeAa_335316
Level 4
Level 4
First like received

 I am developing one device where i need to turn on  LED when signal become high and turn off LED when signal become low .during the LED blinking i have to control the LED light intensity through push up/down botton or  (through capsence).

   

i have attached a jpg of my input signal which is for turn OFF and ON 10 times in 1 sec .

   

0 Likes
1 Solution
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Then I would consider using a comparator (simplest) to detect level

   

and in turn in code use that to enable a PWM. When PWM active

   

use its compare value to control duty cycle, hence brightness of

   

LED.

   

 

   

Set PWM period so that it is ~ 100 Hz or more to avoid flicker in LED.

   

 

   

Note timer would work here as well. Or SSDM module, it will result in

   

better EMI reduction.

   

 

   

Regards, Dana.

View solution in original post

0 Likes
14 Replies
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Describe the input signal, its source if possible, is it AC, DC,

   

freq if AC.

   

 

   

What property of the signal turns LED on or off ? Paek, average, RMS, period.....?

   

 

   

Your input signal pic not showing up in my browsers (Firefox, Chrome).

   

 

   

Regards, Dana.

0 Likes
DeAa_335316
Level 4
Level 4
First like received

 i am using chrome .... already attached one file ....you can download .

   

led should turn on when signal at zero (low) leval .

   

time duration for led turn on and off-- 

   

turn on =0.025 sec

   

turn off=0.045 sec

   

Vpp =2.5v

0 Likes
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

Then I would consider using a comparator (simplest) to detect level

   

and in turn in code use that to enable a PWM. When PWM active

   

use its compare value to control duty cycle, hence brightness of

   

LED.

   

 

   

Set PWM period so that it is ~ 100 Hz or more to avoid flicker in LED.

   

 

   

Note timer would work here as well. Or SSDM module, it will result in

   

better EMI reduction.

   

 

   

Regards, Dana.

0 Likes
DeAa_335316
Level 4
Level 4
First like received

 Hi i am using COMPA comparator ... in below given pics yellow one is my filter output and green one is my caomparator output.

   

but comparator output (green) is flickering too much ...

   

   

for elimination of flicker i am using  RC integrator .after that i am able to get this out put 

   

   

 

   

but actually  i want to eliminate this flicker noise at my out put .... how i can get this out put as i mention below ...

   

   

 

   

 

   

plzz help me to  find out the out put tell me the best way to remove fliker at my out put ..... 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Best for controlling LED intensity is a SSDM component for PSoC1. Use a linear function, input is your button up/down counter, output is the "density" value for SSDM.

   

 

   

Bob

0 Likes
DeAa_335316
Level 4
Level 4
First like received

Dear Bob

   

i trying  to control LED through DAC ... but m not able geting the result  from DAC even basic code is not working  ... m taking VC1 =clk/2 , and output pin is strong ...  

   

CODE-

   

 

   

DAC6_1_Start(DAC6_1_HIGHPOWER);

   

while(1) 

   

if(bDACValue == 0)                

   

     {

   

            bDACValue = DAC_MAX;        // Reset DAC value to the max if it reached zero

   

        }

   

        

   

     DAC6_1_WriteStall(bDACValue--);   // Write value to DAC and decrement

   

    

   
    }   
   
        
   
        
   
    plzz find the attached acrchive ....   
0 Likes
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

If you are using a VDAC driving thru output buffer you will have a

   

very non linear brightness vs V result in LED. Thats why you should

   

use SSDM or PWM. Or convert VDAC to IDAC., which is not a good

   

solution.

   

 

   

www.phys.uconn.edu/~hamilton/phys258/N/led.pdf

   

 

   

   

 

   

This shows I thru LED which is directly proportional to LED brightness.

   

So use of VDAC very limiting.

   

 

   

Regarding your code loop, you very rapidly go from max IDAC to 0, there

   

is no delay, and repeat. So average VDAC is 1/2 Vdd which probably does

   

not push much I thru LED. In any event use of IDAC NOT recommended.

   

 

   

Regards, Dana.

0 Likes
DeAa_335316
Level 4
Level 4
First like received

 Hi dana thanks 

   

but i want to know why you do not want to recommended IDAC for event use ... will you elaborate this ... 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Where are you going to take an IDAC from when driving a non-linear LED?

   

 

   

Bob

0 Likes
DeAa_335316
Level 4
Level 4
First like received

 i have already one output m showing below (green one) ... LED also blinking according to rectanguler pulse ......one side of LED anode pin is connected through rectaguler pulse (which is providing ground) and otherside is connected through Vcc ... i just want to control the (Vcc) voltage or current of cathode side of LED pin by pressing up/down push botton  ...  i don't know which mathod is good  ... when rectanguler pulse providing ground....

   

 

   

 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

As alredy said: use the SSDM module @100kHz and controll the density by API when up/dwn buttons pushed.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
100 sign-ins 5 likes given 1000 replies posted

The reasons you cannot use IDAC are -

   

 

   

1) Max IDAC output is ~ 600 uA, insufficient to run most hi efficiency LEDs

   

to an adequate brightness level.

   

 

   

2) Your Vcc is 3.3V, The complience range of the IDAC is 0 - 2.3 V in that case.

   

Most hi bright LEDs, depending on color, have Vth exceeding 2V, in some case

   

3V. This means you could barely turn on LED because of Vth. And LED to LED

   

variation is horrible, so of the ones you could light up you woud have large

   

brightness variation from one LED to another.

   

 

   

3) A PWM works because you can control the width of the pulse, or duty cycle,

   

of the pulse. That in turn means the average effective DC value of the wavefom

   

can vary from 0 - 100% at the output. If the period of the PWM is ~ > 60 Hz you

   

will not see any flicker. Human eye acts as an integrator, so if you pass a pulse

   

of light to it it will integrate that pulse into an effective average light intensity.

   

 

   

4) The SSDM changes density of pusle train effective doing the same thing as

   

the PWM.

   

 

   

Use the SSDM or a PWM.....

   

 

   

Regards, Dana

0 Likes