Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

gisc_1091076
Level 3
Level 3
10 replies posted 10 sign-ins 5 replies posted

Hello,

I have a problems with the interrupts with psoc5. When i start  the interrupts, after a casual time this interrupts are blocked. Can you help me ? it's urgent! Thanks

I have setted the block this:

Resolution: 8-bit

Implemetation.fixed function

Period:100ms

Capture mode:none

Enable mode:Software only

Run mode: Continuos

Interrupts: On TC

Immagine1.png

I have initialized the interrupts this :

      // Start Global Interrupt

     CYGlobalIntEnable ;

   

    CyDelay ( TIME_5_MS ) ;

   

    /* Start components Interrupt */

    isr_I2C_rd_tmr_StartEx ( isr_I2C_rd_tmr_Interrupt ) ;

      // Avvio l'interrupt per leggere l'I2C

    isr_I2C_rd_tmr_Start ( ) ;    // Start ISR

    // ... e il timer per la lettura del i2C

    I2C_Reader_Timer_Start ( ) ;

   

    isr_I2C_rd_tmr_Enable ( ) ;

Functions interrupts :

CY_ISR(isr_I2C_rd_tmr_Interrupt)

{

    #ifdef isr_I2C_rd_tmr_INTERRUPT_INTERRUPT_CALLBACK

        isr_I2C_rd_tmr_Interrupt_InterruptCallback();

    #endif /* isr_I2C_rd_tmr_INTERRUPT_INTERRUPT_CALLBACK */

    /*  Place your Interrupt code here. */

    /* `#START isr_I2C_rd_tmr_Interrupt` */

    // Leggo lo stato del timer      

    I2C_Reader_Timer_ReadStatusRegister ( ) ; 

   

     // Cancello interrupt pendenti

    // isr_I2C_rd_tmr_ClearPending ( ) ;

   

    #ifdef DEBUG_ON       

    count ++ ;

    // Visualizzo il debug solamente una volta                                   

    printf ( "T:%i\r\n" , count ) ;

    #endif  

        /* `#END` */

}

1 Solution
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
Beta tester First comment on KBA 1000 replies posted

Hi,

I also tried with CY8CKIT-059, and found that

"isr_I2C_rd_tmr_Interrupt" is defined in the auto generated function in "isr_I2C_rd_tmr.c".

And you were calling both

    isr_I2C_rd_tmr_StartEx ( isr_I2C_rd_tmr_Interrupt ) ;

and

    isr_I2C_rd_tmr_Start ( ) ;    // Start ISR

Which I don't think good idea.

So I created following project to test

schematic

001-schematic.JPG

Pins

002-Pins.JPG

main.c

==============

#include "project.h"

#include "stdio.h"

volatile uint32_t count = 0 ;

#define STR_LEN 64

char str[STR_LEN+1] ;

void print(char *str)

{

    UART_PutString(str) ;

}

void cls(void)

{

    print("\033c") ; /* reset */

    CyDelay(100) ;

    print("\033[2J") ; /* clear screen */

    CyDelay(100) ;

}

void splash(void)

{

    cls() ;

    print("PSoC 5LP Interrupt Test ") ;

    snprintf(str, STR_LEN, "(%s %s)\n", __DATE__, __TIME__) ;

    print(str) ;

}

CY_ISR(my_I2C_Timer_isr)

{

    I2C_Reader_Timer_ReadStatusRegister() ;

    count++ ;

}

void init_hardware(void)

{

    UART_Start() ;

    /* Start components Interrupt */

    isr_I2C_rd_tmr_StartEx ( my_I2C_Timer_isr ) ;

   

    I2C_Reader_Timer_Start() ;

   

    CyGlobalIntEnable; /* Enable global interrupts. */

}

int main(void)

{

    uint32_t prev_count = 0 ;

   

    init_hardware() ;

   

    splash() ;

   

    for(;;)

    {

        if (prev_count != count) {

            prev_count = count ;

            snprintf(str, STR_LEN, "count = %d\n", prev_count) ;

            print(str) ;

        }

    }

}

==============

Tera Tem log

(at start)

000-TeraTerm-log.JPG

(current (while I'm typing this))

003-TearTerm-log2.JPG

So far, working.

moto

View solution in original post

3 Replies
Len_CONSULTRON
Level 9
Level 9
Beta tester 500 solutions authored 1000 replies posted

gisc,

I'll make a first attempt to address your question.  If my suggestion is not successful, I may ask for a copy of your project to try to reproduce the issue.

I noticed something in the code you included.  You have a printf() statement within the Interrupt Service Request (ISR).  This is basically not a good idea.  The printf() function is potentially a blocking function.  This means that to print your debugging information, you may be stuck in the interrupt with all other interrupts blocked until the printf() is completed and you return from the isr_I2C_rd_tmr_Interrupt() ISR.

Since this is a debugging code line, comment it out.   Connect an PSoC pin configured as an output on the interrupt line.  See pic.

pastedImage_0.png

Connect an oscilloscope to the Pin_ISR_mon.  You should see a positive pulse every time an ISR is requested.  This is a good HW debugging mode to replace your printf() with no performance impact on your running code.

Len

Len
"Engineering is an Art. The Art of Compromise."
0 Likes
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
Beta tester First comment on KBA 1000 replies posted

Hi,

I also tried with CY8CKIT-059, and found that

"isr_I2C_rd_tmr_Interrupt" is defined in the auto generated function in "isr_I2C_rd_tmr.c".

And you were calling both

    isr_I2C_rd_tmr_StartEx ( isr_I2C_rd_tmr_Interrupt ) ;

and

    isr_I2C_rd_tmr_Start ( ) ;    // Start ISR

Which I don't think good idea.

So I created following project to test

schematic

001-schematic.JPG

Pins

002-Pins.JPG

main.c

==============

#include "project.h"

#include "stdio.h"

volatile uint32_t count = 0 ;

#define STR_LEN 64

char str[STR_LEN+1] ;

void print(char *str)

{

    UART_PutString(str) ;

}

void cls(void)

{

    print("\033c") ; /* reset */

    CyDelay(100) ;

    print("\033[2J") ; /* clear screen */

    CyDelay(100) ;

}

void splash(void)

{

    cls() ;

    print("PSoC 5LP Interrupt Test ") ;

    snprintf(str, STR_LEN, "(%s %s)\n", __DATE__, __TIME__) ;

    print(str) ;

}

CY_ISR(my_I2C_Timer_isr)

{

    I2C_Reader_Timer_ReadStatusRegister() ;

    count++ ;

}

void init_hardware(void)

{

    UART_Start() ;

    /* Start components Interrupt */

    isr_I2C_rd_tmr_StartEx ( my_I2C_Timer_isr ) ;

   

    I2C_Reader_Timer_Start() ;

   

    CyGlobalIntEnable; /* Enable global interrupts. */

}

int main(void)

{

    uint32_t prev_count = 0 ;

   

    init_hardware() ;

   

    splash() ;

   

    for(;;)

    {

        if (prev_count != count) {

            prev_count = count ;

            snprintf(str, STR_LEN, "count = %d\n", prev_count) ;

            print(str) ;

        }

    }

}

==============

Tera Tem log

(at start)

000-TeraTerm-log.JPG

(current (while I'm typing this))

003-TearTerm-log2.JPG

So far, working.

moto

Thanks you , i have resolved the my problem.