Attachments are accessible only for community members.
Anonymous
Not applicable
Nov 01, 2011
05:20 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 01, 2011
05:20 AM
I am using PSOC5 Creator and I need to only raise an interrupt on the Reception of 8 byte data entered from the keybaord and trasferred via serial port interface.However while configuring the Uart block in the Top Design Module, It shows that the Internal Rx Interrupt is disabled and doesn't give me an option to enable it, as a result of which I am unable to use the API command UART_EnableRxInt (void) in the main.c. Please note that I used the Rx only mode and I have checked the Rx-One byte received in the Interrupt Sources option.
Someone please suggest me what to do ? :'(
Labels
- Labels:
-
PSoC 5LP
2 Replies