Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

TaYu_4314136
Level 1
Level 1

My environment is PSoC 5LP(CY8KIT-059/CY8C5888LT) with PSoC Creator 4.2 on Window 10.

I want to read a single wired serial signal from GPIO with UDP.

First, I wrote a program that doesn't require an external input.

画像5.png

(*USB clock is for future implementation)

circuit.png

`include "cypress.v"

module data_in_test (
    input data_in,
input   clock,
    output  dma
);

wire op_clk;
parameter  ClockSyncMode = 1'b1;
cy_psoc3_udb_clock_enable_v1_0 #(.sync_mode(ClockSyncMode)) ClkSync
(
    .clock_in(clock),
    .enable(1'b1),
    .clock_out(op_clk)
);    

localparam RG_IDLE = 3'b000;
localparam RG_SHIFT = 3'b001;
reg [2:0]rg_state;

reg dp_f0_load;
reg[2:0] state;
reg[3:0] ct;

wire dp_si;
reg dp_si_reg;
assign dp_si = dp_si_reg;

always @(posedge op_clk)
begin
    dp_si_reg <= ~dp_si_reg;
    dp_f0_load <= 1'b0;
    rg_state <= RG_SHIFT;
   
    ct <= ct + 1'b1;
    if(ct == 1'b0)
    begin
        dp_f0_load <= 1'b1;
    end
end

cy_psoc3_dp8 #(.cy_dpconfig_a(
{
    `CS_ALU_OP_PASS, `CS_SRCA_A0, `CS_SRCB_D0,
    `CS_SHFT_OP_PASS, `CS_A0_SRC_NONE, `CS_A1_SRC_NONE,
    `CS_FEEDBACK_DSBL, `CS_CI_SEL_CFGA, `CS_SI_SEL_CFGA,
    `CS_CMP_SEL_CFGA, /*CFGRAM0:  */
    `CS_ALU_OP_PASS, `CS_SRCA_A0, `CS_SRCB_D0,
    `CS_SHFT_OP___SL, `CS_A0_SRC__ALU, `CS_A1_SRC_NONE,
    `CS_FEEDBACK_DSBL, `CS_CI_SEL_CFGA, `CS_SI_SEL_CFGA,
    `CS_CMP_SEL_CFGA, /*CFGRAM1:  */
    `CS_ALU_OP_PASS, `CS_SRCA_A0, `CS_SRCB_D0,
    `CS_SHFT_OP_PASS, `CS_A0_SRC_NONE, `CS_A1_SRC_NONE,
    `CS_FEEDBACK_DSBL, `CS_CI_SEL_CFGA, `CS_SI_SEL_CFGA,
    `CS_CMP_SEL_CFGA, /*CFGRAM2:  */
    `CS_ALU_OP_PASS, `CS_SRCA_A0, `CS_SRCB_D0,
    `CS_SHFT_OP_PASS, `CS_A0_SRC_NONE, `CS_A1_SRC_NONE,
    `CS_FEEDBACK_DSBL, `CS_CI_SEL_CFGA, `CS_SI_SEL_CFGA,
    `CS_CMP_SEL_CFGA, /*CFGRAM3:  */
    `CS_ALU_OP_PASS, `CS_SRCA_A0, `CS_SRCB_D0,
    `CS_SHFT_OP_PASS, `CS_A0_SRC_NONE, `CS_A1_SRC_NONE,
    `CS_FEEDBACK_DSBL, `CS_CI_SEL_CFGA, `CS_SI_SEL_CFGA,
    `CS_CMP_SEL_CFGA, /*CFGRAM4:  */
    `CS_ALU_OP_PASS, `CS_SRCA_A0, `CS_SRCB_D0,
    `CS_SHFT_OP_PASS, `CS_A0_SRC_NONE, `CS_A1_SRC_NONE,
    `CS_FEEDBACK_DSBL, `CS_CI_SEL_CFGA, `CS_SI_SEL_CFGA,
    `CS_CMP_SEL_CFGA, /*CFGRAM5:  */
    `CS_ALU_OP_PASS, `CS_SRCA_A0, `CS_SRCB_D0,
    `CS_SHFT_OP_PASS, `CS_A0_SRC_NONE, `CS_A1_SRC_NONE,
    `CS_FEEDBACK_DSBL, `CS_CI_SEL_CFGA, `CS_SI_SEL_CFGA,
    `CS_CMP_SEL_CFGA, /*CFGRAM6:  */
    `CS_ALU_OP_PASS, `CS_SRCA_A0, `CS_SRCB_D0,
    `CS_SHFT_OP_PASS, `CS_A0_SRC_NONE, `CS_A1_SRC_NONE,
    `CS_FEEDBACK_DSBL, `CS_CI_SEL_CFGA, `CS_SI_SEL_CFGA,
    `CS_CMP_SEL_CFGA, /*CFGRAM7:  */
    8'hFF, 8'h00,  /*CFG9:  */
    8'hFF, 8'hFF,  /*CFG11-10:  */
    `SC_CMPB_A1_D1, `SC_CMPA_A1_D1, `SC_CI_B_ARITH,
    `SC_CI_A_ARITH, `SC_C1_MASK_DSBL, `SC_C0_MASK_DSBL,
    `SC_A_MASK_DSBL, `SC_DEF_SI_0, `SC_SI_B_DEFSI,
    `SC_SI_A_ROUTE, /*CFG13-12:  */
    `SC_A0_SRC_ACC, `SC_SHIFT_SL, 1'h0,
    1'h0, `SC_FIFO1_BUS, `SC_FIFO0__A0,
    `SC_MSB_DSBL, `SC_MSB_BIT0, `SC_MSB_NOCHN,
    `SC_FB_NOCHN, `SC_CMP1_NOCHN,
    `SC_CMP0_NOCHN, /*CFG15-14:  */
    10'h00, `SC_FIFO_CLK__DP,`SC_FIFO_CAP_AX,
    `SC_FIFO_LEVEL,`SC_FIFO__SYNC,`SC_EXTCRC_DSBL,
    `SC_WRK16CAT_DSBL /*CFG17-16:  */
}
)) dp(
    .reset(1'b0),
    .clk(op_clk),
    .cs_addr(rg_state),
    .route_si(dp_si),
    .route_ci(1'b0),
    .f0_load(dp_f0_load),
    .f1_load(1'b0),
    .d0_load(1'b0),
    .d1_load(1'b0),
    .f0_bus_stat(dma),
    .f0_blk_stat(),
    .f1_bus_stat(),
    .f1_blk_stat()
);
endmodule

#include "project.h"
#include <stdio.h>

/* Defines for data_in_dma */
#define data_in_dma_BYTES_PER_BURST 1
#define data_in_dma_REQUEST_PER_BURST 1
#define data_in_dma_SRC_BASE (CYDEV_PERIPH_BASE)
#define data_in_dma_DST_BASE (CYDEV_SRAM_BASE)

/* Variable declarations for data_in_dma */
/* Move these variable declarations to the top of the function */
uint8 data_in_dma_Chan;
uint8 data_in_dma_TD[1];

#define COUNT 256
uint8 res_buffer[COUNT];

void InitDma()
{
    /* DMA Configuration for data_in_dma */
    data_in_dma_Chan = data_in_dma_DmaInitialize(data_in_dma_BYTES_PER_BURST, data_in_dma_REQUEST_PER_BURST,
        HI16(data_in_dma_SRC_BASE), HI16(data_in_dma_DST_BASE));
    data_in_dma_TD[0] = CyDmaTdAllocate();
    CyDmaTdSetConfiguration(data_in_dma_TD[0], COUNT, data_in_dma_TD[0], data_in_dma__TD_TERMOUT_EN | CY_DMA_TD_INC_DST_ADR);
    CyDmaTdSetAddress(data_in_dma_TD[0], LO16((uint32)data_in_test_1_DMA_PTR), LO16((uint32)res_buffer));
    CyDmaChSetInitialTd(data_in_dma_Chan, data_in_dma_TD[0]);
    CyDmaChEnable(data_in_dma_Chan, 1);
}

int out_once_check = 0;

CY_ISR(OnInterruptPaInDma)
{
    if(out_once_check) return;
    out_once_check = 1;
   
    for(int n = 0; n < COUNT; n++){
        for(int m=0;m<8;m++){
            UART_PutChar(((res_buffer >> (7-m)) & 0x1) ? '1' : '0');
        }
        UART_PutChar('\n');
    }
}

int main(void)
{
    CyGlobalIntEnable;

    isr_dma_StartEx(OnInterruptPaInDma);
    InitDma();
   
    UART_Start();

    for(;;)
    {
    }
}

It works well.

1010.png

Next, I sent a signal of 6 MHz to P3[0] pin like this.

ask.png

This is a sample of the result.

0010.png

Considering that a clock source for sync is 24 MHz the same value should continue for two(110011110011...) even if there is a slight synchronization deviation. That is, it can't acquire data by a sync clock. I also connected PSoC standard filter and sync components, but there was no effect.

This is a full project on OneDrive. Please tell me what is missing in my project

1 Solution

tayuc,

I am thinking of different approach: the PSoC5 PLL can be locked to incoming external 6MHz SPDIF signal, then the data can be read directly using FIFO buffer and DMA. This is just an idea.

/odissey1

P.S. I tried to lock PSoC5 PLL to external SPDIF signal (clocked at 6MHz). The resulting PLL output frequency got same as the input, but does not phase-lock to ~2MHz SPDIF signal due to high instability of the signal. Reducing PLL current down to 1uA hepls, but PSoC5 has no lower current settings. I see potential solution using external 4046 PLL for extracting 6MHz carrier from SPDIF signal and then locking PSoC5 PLL to that carrier.

View solution in original post

0 Likes
5 Replies
NoriTan
Employee
Employee
10 sign-ins First question asked 5 sign-ins

I have a comment to your code.

reg[3:0] ct;

:

always @(posedge op_clk) 

:

begin 

    ct <= ct + 1'b1; 

    if(ct == 1'b0)  

    begin 

:

    end 

end 

At first you declare the register ct as reg[3:0] the ct becomes a 4-bit register.

You compare the register ct with 1'b0, but 1'b0 is expanded to 4-bit 4'b0000 as well as the incrementa 1'b1 is expanded to 4'b0001 i line 06

As the result the line 09 is executed every 16 clocks because ct is declared as 4-bit register.

If you want to assert f0_load every 8 clocks,  Use 3-bit register as ct.

Regards,

Noriaki

0 Likes
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

TaYu,

It seems that you are trying to read a serial signal. Did you try to use a standard UART? With oversampling 8x it should handle 6MHz carrier. 

0 Likes
TaYu_4314136
Level 1
Level 1

Originally is S/PDIF. I tried with 12.288MHz crystal x4 PLL referring to Cypress's SPDIF_Tx sample includes in PSoC Creator, but failed.

For this reason, to make a program that solves this noise, I use pseudo signals instead of.

> reg[3:0] the ct becomes a 4-bit register.
It's my easy mistake. thanks for your advice.

I uploaded a latest archive. A result is close to that in the logic analyzer, but it still contains noise.

8bit.png

0 Likes

tayuc,

I am thinking of different approach: the PSoC5 PLL can be locked to incoming external 6MHz SPDIF signal, then the data can be read directly using FIFO buffer and DMA. This is just an idea.

/odissey1

P.S. I tried to lock PSoC5 PLL to external SPDIF signal (clocked at 6MHz). The resulting PLL output frequency got same as the input, but does not phase-lock to ~2MHz SPDIF signal due to high instability of the signal. Reducing PLL current down to 1uA hepls, but PSoC5 has no lower current settings. I see potential solution using external 4046 PLL for extracting 6MHz carrier from SPDIF signal and then locking PSoC5 PLL to that carrier.

0 Likes

Dear BoTa.

It's very helpful how to create a clock with 74HC4046.

The pseudo signal has a limit in development. So I created an environment that receiving the actual 48KHz audio signal with 12.288 MHz crystal.  However, PSoC seems to be operating at a different frequency than the clock source(Both XTAL / Digital Signal).

This is an issue about a clock generator not UDP, so I'll ask about this at a new thread if necessary.

0 Likes