Sep 17, 2020
07:44 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 17, 2020
07:44 AM
I'm working with PSOC 3 device through SWD interface using third side hardware.
So I have access to PSOC registers and can use WRITE_REGISTER(<ADDR>,<DATA>) and READ_REGISTER (<ADDR>) commands.
The task is to define I2C pins pair different from default.
How can I do it?
Solved! Go to Solution.
Labels
- Tags:
- mcu & psoc: psoc 3
1 Solution
Oct 07, 2020
06:35 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Oct 07, 2020
06:35 AM
Hi LeKu_697901,
I am sorry for the delay in my response. Unfortunately, there is no direct way to get the registers that need to be configured. One thing that can be done is to create a PSoC Creator project for the same functionality and backtrack the registers using the source code that is generated. Would it be okay to use the PSoC Creator project directly to test the I2C functionality?
Thanks and Regards,
Rakshith M B
Thanks and Regards,
Rakshith M B
Rakshith M B
6 Replies