Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

Erka_3237036
Level 3
Level 3
5 likes given First like received First like given

Hello,

      

            i have Varitronix MGLS24064  graphical display and i want to interface with psoc 5 lp . please guide me on to this .

and suggest me the example code for this .

  Best Regards,

  Seggi.

0 Likes
1 Solution

It seems that the MGLS24064   uses the TOSHIBA controller T6963C.

It is similar to PG 12864 and WG240128R-TFH which I tested.

(pins 11-20  are biased and a different screen size  )

I have old examples of working with them, maybe this will help you at the beginning of the path:

WG240128_5LP.zip  this is here

GLCD_1WIRE.zip   it is here

LCD128X64.cylib GLCD_DMA.cylib it is here
Evgeniy

View solution in original post

0 Likes
3 Replies
Len_CONSULTRON
Level 9
Level 9
500 solutions authored 1000 replies posted 750 replies posted

Seggi,

The CY8CKIT-050 has a LCD display very similar interface to your Varitronix MGLS24064 graphical display.

You can probably use the code examples for this kit as a good starting point.

Len

Len
"Engineering is an Art. The Art of Compromise."
0 Likes

Hello LePo,

                  i think i was interfaced  this graphical LCD with the psoc 5 LP is successfully. but i am going to print some numbers and string they can't print on my LCD. as per our old codes i am going for same as the LCD codes i.e. initialize LCD after initialization ,position and last string or number whatever i want to print but in this LCD i don't know how to give the positions and how to print the string and numbers.

one more thing psoc is already giving the Top Design but i don't know they are giving some pins like read write chip select or data command

how can i pass value on it .

i'll give you the pin numbers what i has used please let me know those are right or wrong.

WR ---> P12[7]

RD  ---> P12[6]

CE  ---> P12[5]

C/D ---> P12[4]

DB0-DB7 ---> P5[7:0]

and i don't Know should i do for Vo pin?

can you give me some example code for this it would be more helpful to me . Thanks in advanced

Thank you ,

Best Regards,

Seggi.

0 Likes

It seems that the MGLS24064   uses the TOSHIBA controller T6963C.

It is similar to PG 12864 and WG240128R-TFH which I tested.

(pins 11-20  are biased and a different screen size  )

I have old examples of working with them, maybe this will help you at the beginning of the path:

WG240128_5LP.zip  this is here

GLCD_1WIRE.zip   it is here

LCD128X64.cylib GLCD_DMA.cylib it is here
Evgeniy

0 Likes