Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

I have a question about how to adjust the ADC.

what should the setting be if you have to measure a
signal on an input that has a value between 3 and 4 volts.

And the required measurement accuracy must be 0.5mV.

1 Solution

hmeijerink,

one way to accomplish this is to use ADC_SAR in differential mode, providing V(-) terminal with offset voltage 3.5V. To make full scale 1V, the ADC_SAR Vref voltage must be 500mv (full scale is 2xVref), which can be provided by VDAC. Schematic is attached. Note that due to the electrical noise in the system, the ADC reading fluctuate approx. 5-10 counts (full scale 4096), to get to 1-2 counts a low-noise power supply and caps required, plus some ADC averaging. P.S. What data acquisition rate you need?

/odissey1

ADC_SAR_3-4V_1a.png

ADC_SAR_3-4V_1b.png

View solution in original post

0 Likes
5 Replies
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

What ADC will be used ADC_SAR or DelSig_ADC?

/odissey1

0 Likes
Anonymous
Not applicable

I used the ADC_SAR

0 Likes

hmeijerink,

one way to accomplish this is to use ADC_SAR in differential mode, providing V(-) terminal with offset voltage 3.5V. To make full scale 1V, the ADC_SAR Vref voltage must be 500mv (full scale is 2xVref), which can be provided by VDAC. Schematic is attached. Note that due to the electrical noise in the system, the ADC reading fluctuate approx. 5-10 counts (full scale 4096), to get to 1-2 counts a low-noise power supply and caps required, plus some ADC averaging. P.S. What data acquisition rate you need?

/odissey1

ADC_SAR_3-4V_1a.png

ADC_SAR_3-4V_1b.png

0 Likes
Anonymous
Not applicable

Thank you for your explanation this was a question for school to understand the ADC

0 Likes

hmeijerink,

Theoretically speaking, I believe that you need Diff Amp to scale input voltage by 2 and shift it down to ADC range 0-2.048V. Figure (A) shows example of standard DiffAmp, which accomplishes that, which can be reduced to form (B) (inverted amplifier) or form (C) (standard diff amp). Drawbacks (B) - inverted ADC input, (C) - requires precision matched resistors, which would be hard to achieve using PSoC internal opamp due to trace resistance. For the future, please post academic questions elsewhere (stackoverflow / stackechange). A good resource for reading about real OpAms and ADCs:

Analog Engineer’s Circuit Cookbooks | Op Amp Circuits | ADC Circuits | TI.com

/odissey1

DiffAmp_1a.png

DiffAmp_1b.png

DiffAmp_1c.png

0 Likes