cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

AmCi_3754291
New Contributor

Hey,

I have a board that has SCL connections to pins 49 and 60 and SDA connections to pins 53 and 61. I am trying to connect all 4 of these pins to the same I2C Master block. Is this possible? If so How do I do it?

I tried the design in the image, but that complains that the lines are driven more than once

Thanks

Amilcar

0 Likes
1 Solution
MotooTanaka
Esteemed Contributor

Hi,

Assuming that you are using LOGO for monitoring (output),

I could generate application with following schematic.

000-schematic.JPG

Note: The triangle is "Digital > Logic > Bufoe" and LOGO pins are "Bidirectional, Strong Drive"

Note2: I have not tested if it works or not.

moto

View solution in original post

0 Likes
1 Reply
MotooTanaka
Esteemed Contributor

Hi,

Assuming that you are using LOGO for monitoring (output),

I could generate application with following schematic.

000-schematic.JPG

Note: The triangle is "Digital > Logic > Bufoe" and LOGO pins are "Bidirectional, Strong Drive"

Note2: I have not tested if it works or not.

moto

View solution in original post

0 Likes