cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

seku_495601
New Contributor II

How can Change Filter Co-eff During Run Time in PSOC5 LP Filter Block? any Examples

0 Likes
5 Replies
Vasanth
Moderator
Moderator

Hi,

Please checkout one way to do it. A function can be written for the purpose.

NOTE: Using this function requires the filter component to be set up with the same
type of filter (biquad or FIR) and number of taps/order as the coefficients being
loaded here.

*/
void Filter_LoadCoefficients(uint8 *pFiltCoeffs, uint16 wSize, uint16 wOffset) 
{
	/* This is the externally defined null array we will 
	use to clear out the sample data in RAM */
	extern const uint8 CYCODE Filter_data_a[];
	
    /* Power on DFB before initializing the RAMs */
    Filter_PM_ACT_CFG_REG |= Filter_PM_ACT_MSK;

    /* Turn off Run Bit */
    Filter_CR_REG &= ~Filter_RUN_MASK;
                
    /* Enable the DFB RAMS */
    Filter_RAM_EN_REG = Filter_RAM_DIR_BUS;
        
    /* Put DFB RAM on the bus */
    Filter_RAM_DIR_REG = Filter_RAM_DIR_BUS;
        
    /* DAta RAMs */
	
    /* Clear out the RAM which contains the sample values 
	from the previously operating filter */
	memcpy(Filter_DA_RAM,
        Filter_data_a, Filter_DA_RAM_SIZE); 
    
	/* This one copies wSize bytes of filter coefficients at the specified offset in the data B RAM  */
	memcpy(Filter_DB_RAM+wOffset,
        pFiltCoeffs, wSize); 

    /* Take DFB RAM off the bus */
    Filter_RAM_DIR_REG = Filter_RAM_DIR_DFB;

    /* Set up interrupt and DMA events */
//    Filter_SetInterruptMode(Filter_INIT_INTERRUPT_MODE);
//    Filter_SetDMAMode(Filter_INIT_DMA_MODE);
        
    /* Clear any pending interrupts */
    /* Bits [2..0] of this register are readonly. */
    Filter_SR_REG = 0xf8;   
}

Best Regards,
Vasanth

 

seku_495601
New Contributor II

My Co-eff are as follows

 

Final coefficients for Biquad filter :
Coefficients are in the order A0, A1, A2, B1 and B2

0.24254298210144
-0.485085725784302
0.24254298210144
-1.93959474563599
0.941091299057007

0.966162204742432
-1.93232417106628
0.966162204742432
-1.93157911300659
0.933069467544556

0.963419437408447
-1.92683911323547
0.963419437408447
-1.92609620094299
0.927582025527954

0.962027311325073
-1.92405486106873
0.962027311325073
-1.92331290245056
0.92479681968689

0.975322961807251
-1.9506459236145
0.975322961807251
-1.94989371299744
0.951398134231567

0.981450796127319
-1.96290183067322
0.981450796127319
-1.96214485168457
0.963658571243286

0.988350868225098
-1.97670149803162
0.988350868225098
-1.97593927383423
0.977463722229004

1.99156522750854
-3.98313045501709
1.99156522750854
-1.99079728126526

 

How can i use that one?  what is Offset  Value?

0 Likes
Len_CONSULTRON
Honored Contributor II

seku,

Are you talking about the Digital Filter Block (DFB) or the analog Low-pass filters (LPF)?

Len
"Engineering is an Art. The Art of Compromise."
0 Likes
ARH
New Contributor II

Im just glad to see that someone is using the DFB... 

0 Likes
seku_495601
New Contributor II

i Need Both example with Dynamic Loading or changing Filter Co-eff

0 Likes